Other Parts Discussed in Thread: TPS56121, TPS62130, TPS55386, TPS54386, TPS53353
请问实现如下功能的有什么IC:
1、IN:12V DC OR 5V,OUT:+3.3V/3A
2、IN:12V DC OR 5V,OUT:+1.0/11.65A
3、IN:12V DC OR 5V,OUT:+1.8V/0.7A
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
在TI的电源官网:www.ti.com.cn/.../power_portal.page 有"电源快速搜索"功能,在此表中输入您要的设计参数(可选择两路输出的),就可以搜索出非常多的适合您应用的芯片,然后您在精确挑选(可以从价格,layout面积,复杂程度,效率等方面)
例如TPS54386/TPS55386 可以实现2路输出 3.3V/3A, 1.8V、0.7A.
5~12V(或者5V/12V)输入,选择TPS56121, TPS53353都是可以实现1V/11.65A输出的。