想给正在制作中的红外遥控器装三节7号AAA电池来作电源
故会需要把3.3v~4.5v的输入电源转成稳定的3.3v给MSP430G2553以及蓝牙模块HC-06(待机时断电)用
并且待机功耗(<10uA)时的转换效率还可以的稳压IC
已经找到有LP2951、LM3480-3.3、LM3940这几个LDO
只是不知道哪款会比较适合这样低功率的使用情况
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
电流需求是多大?
空间够不够,是否可以用DC/DC? 这样电池应用时间更长。
您好,TPS783的输入范围是2.2--5.5V,那它的输出电压是稳定的3.3V吗?
如果你输入大于3.3V,输出是可以在3.3V,这个LDO的压降为130mV,所以当输入小于3.43V,输出就会相应降低