This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24040 静态功耗问题请教

Other Parts Discussed in Thread: BQ24040

你好,我想请教一下以下问题,谢谢:

1. 在Vin为0,电池有接入的情况下,ISET, ISET2, PRETERM, TS上的端接电阻是否会消耗电流? 尤其是TS,如果我外部一直接着电池的NTC,或者一直有10K电阻下拉,那么他上面是否一直会消耗50uA的电流,即便是系统待机的情况下。

2. spec上描述,静态电流Iout(done)在VIN=6V, Vout>Vout(reg)下是6uA,我不是很理解Vout>Vout(reg)是什么样一个状态,BQ24040的Vout(reg)是指稳压器的默认输出,典型值是4.2V,Vout是Vout上的实际电平。 正常情况下应该不会有Vout>Vout(reg)的场景吧,那么这个参数的意义何在?

3. CHG 只在第一次充电为低电平。假设我一直插着充电器充满后,由于系统负载比较大,VOUT电压掉到VRCH以下,BQ24040又开始充电直到,那么我的系统是否永远不知道电池还在充电,甚至充满了呢(读取CHG)?  是否只有Vin重新上下电之后,CHG才会在充电时变低?