Other Parts Discussed in Thread: BQ27210
保护板采用bq27210(3.7V/890mAH)设计,电池learning后开路电压为3.95V左右,剩余容量百分比为65%~70%之间,电池搁置5个月后剩余容量百分比降至50%左右(按照设计0.2%以内自耗电计算正常),但开路电压只降低2~3mv(3.9V左右),不知道如何从专业的角度去解释这个问题(客人的问题就是为什么电量掉了这么多而电压却只掉了一点点?)
以上,谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
River,
不同品牌的电池开路电压曲线会不同,很难说某一开路电压具体对应多少的剩余容量,必须使用高精度测试仪来测试近似的开路电压曲线才能得出电压与容量关系。bq27210里对于自放电仅仅是使用0.2%/天的参数来线性模拟容量的衰减,有些好的电池月自放电率小于2%,故也可能是bq27210里对自放电率的设定过于保守,可以设定更小一点。建议测试下电池包的功耗,如果你指的2~3mV压降是准确的,电池包的功耗估计就在2uA,你可以拿只剩50%电量的电池包放电到空,如果放电电量明显大于50%,也可以说明是bq27210里自放电率设定较大,可以调小一些。
Luke