This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5181-Q1: 7路输出变压器设计,峰值电流以及励磁感量的计算

Part Number: LM5181-Q1


Hi TI的专家,

目前我们正计划使用LM5181-Q1作为驱动变压器的IC,

目前驱动变压器的应用信息为:

Vin=9V-28V,Vin_norminal=12V 

Vout1,3,5=19V / Iout1,3,5=0.05A,Vout2,4,6=-4V / Iout2,4,6=-0.01A,

Vout7=5V /  Iout7=0.02A

共7路输出,总输出功率≈3.1W

我们设定占空比为0.4,匝比:Np/NS1,3,5(19V)=0.3, Np/NS2,4,6(-4V)=1.3, Np/NS7(5V)=1.0  AT Vinmin=9V

问题1:当我们使用规格书中公式计算峰值电流时,初级峰值电流为1.783A,远大于我们集成mos管中的0.75A峰值电流限制,请问是我们计算有误,还是此应用条件不适用于此款IC

问题2:当我们使用规格书中计算最小励磁感量为100uH, 如此大的励磁感量就会造成需要非常多的初级圈数,造成变压器尺寸会远大于常规3.1W输出功率所设配的尺寸,请问我们计算是否有误,或则我们是否可以降低这个励磁感量

盼复,谢谢!