Other Parts Discussed in Thread: BQ24070
请帮忙推荐一款锂电池充电IC,要求如下:
IC的输入电压:5V或者12V
输出电压:4.2V
而且外部输入电源(如AC适配器即充电IC的输入端)在给锂电池充电的同时也可以给后端工作系统供电;锂电池不需充电时只给后端供电;无外部输入电源(AC适配器)时锂电池给后端供电;
后端负载要求:工作电压4.2V,电流2A
请问BQ24070芯片是否符合要求?如不符合请给推荐合适的芯片。谢谢,急需答案!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
同时考虑到BQ24070是线性充电器,所以它更适合5V输入的场合,如果输入电压源可能比较长时间的出现12V,或者直接使用固定12V的电源,那么需要换用一个开关模式的充电器,否则使用BQ24070效率太低(vout/VIN),芯片消耗功耗太大发热Ploss=Iout*(Vin-Vout),以上谢谢!