工程师:
你好,初次使用TI的DCDC升压芯片,现在对TPS1030升压芯片,我想从3.3v~5.5v升压到4.2v,现有以下几个问题:
1、TPS1030升压芯片输出4.2v的电压,可以持续输出3A的电流吗?芯片不会因电流过高,而烧坏把?
2、TPS1030升压芯片可以工作在省电模式,请问这个模式下输出的电压和电流不会改变吧?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
TPS61030是升压芯片,并不带降压部分,所以要输出4.2V, 输入需要小于4.2V.
同时这是芯片开关电流是3.6A, 3.3V输入时最大输入电流大约是3.6/1.2=3A, 按照85%的效率,最大输出电流大约是3.3*3*0.85/4.2=2A
Powersaving模式主要是提升轻载时效率,输出电压是稳定的。
Hi
你需要的最大输出电压是3A吗? 输入电压是否可以调整,因为要选升降压型的芯片做到3A最大输出是乎只能选择外部MOS的芯片。
Hi
你好,我这边用的锂电池,锂电池电压是3.6~4.2v作为输入,希望在3.6v时候还可以得到4.2v电压,工作电流2A左右,峰值电流3A。能不能推荐一个升压芯片?(方便的话加你一下QQ,我的QQ:634922687)
Hi
选择TPS55330: http://www.ti.com/product/TPS55330
你好,问一下TPS61030升压芯片,如果我想要输出的4.2v电压,如果我输入超出4.2v是不是输出也超出4.2v,假如输入5v,是不是输出也是5v?
楼主,
当输入大于输出时,基本上MOS管已经关断,此时,输入会直通到输出,输出也会跟随输入的上升而上升。不过此时输出电压VO=VIN-VDROP,此处VDROP包括了二极管的正向压降,电流在电感直流阻抗上产生的压降,以及线路阻抗中产生的压降。
你好,问一下TPS55330的功耗高不高,输入3.6~4.2v之间输入,输出4.2v的效率高不高?
楼主,整个升压变换器的效率与你选择的输出二极管,电感等都有很大关系,如果单单是TPS55330,在boost不使能时,芯片自耗电2.7uA,如果是空载输出,芯片自耗电0.5mA.具体整体变换器的效率可以参考一下规格书第一页的效率曲线,或者是EVM的user guide里面的测试数据。
谢谢,这么晚还回复,我看了一下TPS55330的使用手册,其实我认为TPS61030比较使用于锂电池,我想让你在帮我计算一下TPS1030在3.6~4v之间升压到4.2v,输出的电流可以持续在1.5A吗,如果可以我就选用这个TPS61030,因为TPS61030具有低压锁定功能。