在UC2844的芯片资料中可以查到,UC2844工作温度范围“-40~85℃”,最大结温Tjmax“150℃”。而UC2844的“电气特性表”中测量的条件是“Tj=Ta”,也就是说 说有特性都是在Tj=-40~85℃条件下测量得到的。那么芯片UC2844实际工作环境温度为60℃,Tj=100℃就不符合其“电气特性表”了,那么这种情况下 我还能使用UC2844么,难道必须使用UC1844?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.