This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,主要要求输出电压、电流稳定。TPS562200的输出电流2A,是指最大值2A?还是只能输出2A?
我查到TPS62160系列,和您说的型号哪个比较好?
HI
都可以, 2A是最大输出电流。
选TPS62160系列的TPS62140是可以的,也是2A最大输出。
Hi
都可以, 相比之下TPS62140功能更多。例如Powersaving模式下效率更加高,Powergood功能,还有Powerpad设计,散热也好一些。
但是如果不考虑这些TPS562200也可以用。
你好,当然是最大值2A,你想输出1A也可以,其实最大2A也不是绝对的,这跟你的选的电感也有关系,谢谢。