This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

锂电池充电IC的输出电压偏大了

Other Parts Discussed in Thread: BQ24072T

接续前面的帖子“求推荐锂电池充电IC”,本来想用BQ24070来实现的,但是后端应用的负载(扫网模块)换了,其工作电压在3.6-4.2V,而我选的BQ24070的输出电压为4.4V ,现在应该怎么办呢?4.4V转4.2V?还是换类似得充电IC呢?什么型号更为合适呢?

要求如下:

IC的输入电压:5V或者12V

输出电压:4.2V

具有动态管理功能,外部输入电源(如AC适配器即充电IC的输入端)在给锂电池充电的同时也可以给后端工作系统供电,锂电池不需充电时只给后端供电;无外部输入电源(AC适配器)时锂电池给后端供电;

后端负载要求:工作电压3.6-4.2V,电流2A

谢谢,急需答案!