Part Number: LM317
Other Parts Discussed in Thread: LM337
Hello!
The LM317 and LM337 chips, both packaged in TO-263-3, have similar functions and circuits. However, the second pin of the LM317 is an OUTPUT, while the second pin of the LM337 is an INPUT. I would like to ask if there is an issue with the datasheet or if this is the intended design?
Thank you very much for your reply!
Best regards!
您好!
封装为TO-263-3的LM317和LM337两款芯片功能类似、电路类似,而LM317的二号引脚为OUTPUT、LM337的二号引脚为INPUT,请问是数据手册出现问题还是正是如此设计?
非常感谢您的回复!
祝好!