This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS1H100-Q1: 您好,问一下Internal Current limit写着7~13A,Current limit during thermal shutdown 5A,这两项有什么区别?

Part Number: TPS1H100-Q1

您好,问一下Internal Current limit写着7~13A,Current limit during thermal shutdown 5A,这两项有什么区别?

  • 您好

    内部电流限制是在器件正常工作时的保护阈值,而热关断期间的电流限制则是为了在器件过热时提供一种自我保护机制,确保安全运行

    Internal Current Limit (7~13A): 这个参数指的是在正常工作条件下,用户可以根据需要,设定功率FET的电流上限,通常范围在7到13安培之间。这个设置确保了在负载电流达到预设值时,开关会限制电流以防止过热或损坏负载。

    Current Limit during Thermal Shutdown (5A): 当TPS1H100-Q1由于过热进入热关断状态时,在热关断期间,为了防止进一步的温度上升,器件会将电流限制在5A。这个限制是为了在器件温度过高时,减少功耗,允许器件冷却下来,从而保护器件不被永久损坏。