Other Parts Discussed in Thread: UCC28070,
早上好!想了解一下,交错工作方式下,UCC28070设置频率为130K的话(RT=56.2K),那么GDA、GDB输出的方波频率是130K还是65K?我现在测量是130K?交错方式不是轮流工作,应该为65K吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
早上好!想了解一下,交错工作方式下,UCC28070设置频率为130K的话(RT=56.2K),那么GDA、GDB输出的方波频率是130K还是65K?我现在测量是130K?交错方式不是轮流工作,应该为65K吗?
UCC28070A 振荡器的开关频率由 RT 引脚上的计时电阻器通过数据表中的公式(3)进行设置。 通过 Re 排列方程(3)我们可以得出这样的结果
fPWM (kHz)= 7500/RT (KR)= 7500/56.2 = 133.5kHz。
该频率适用于 GDA 和 GDB。 而不是65kHz。
根据公式(3)、GDX 输出脉冲的前沿时序相移180度、但频率相同。