Other Parts Discussed in Thread: MSP430F149, TPS63051
我用一节锂电池(标称3.7V,范围3.0-4.2V)给MSP430F149(1.8~3.6V)供电,他们之间还需要加入稳压芯片么?需要的话选择什么电路或者芯片呢?设备需要低功耗,所以尽量减少多余的耗电器件为原则。多谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: MSP430F149, TPS63051
我用一节锂电池(标称3.7V,范围3.0-4.2V)给MSP430F149(1.8~3.6V)供电,他们之间还需要加入稳压芯片么?需要的话选择什么电路或者芯片呢?设备需要低功耗,所以尽量减少多余的耗电器件为原则。多谢
Hi
MSP430F149(1.8~3.6V)供电, 一般选择3.3V供电, 电池供电范围可以选择2.5~4.2V, 所以你需要选择一个升降压芯片例如TPS63051之类:http://www.ti.com/product/TPS63051
您好,既然MSP430F149的电池供电电压范围可以使2.5~4.2V,那我选择的电池电压范围是3.0~4.2V,不是正好符合么?为什么还要在电池和芯片之间增加一个生降压芯片呢?
HI
MSP430F149的供电电压是个固定电压,例如3.3V, 选择升降压芯片是为了更加充分利用电池。
当然如果你选择输入电压范围是3.5~4.2V, 选择降压芯片甚至LDO都是可以的。
您好,我看了您给我提供的TPS63051升降压芯片,描述中“ 输出电流在升压模式中会高达 500mA,而在降压模式中会高达 1A。”这样采用一节锂电池(2600MAH),会不会功耗很高呢?
Hi
这个是最大输出电流,实际输出电流和负载有关。