Part Number: TPS25751
TPS25751的湿度检测能帮忙详细描述下是如何实现的吗?下面规格书的这块没有看懂,非常感谢!

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好
原理简单地说是TPS25751通过将SBU线驱动到已知电压并测量它们是否处于预期电压来实现液体检测。检测采样间隔为一定的睡眠时间。每次看到NMOS/PMOS线切换时,都是检测采样阶段。只有在取样阶段才会检测到液体。因此,在9-16中,您最初会看到PMOS/NMOS驱动器切换,同时看到sbu线切换。在大约47.2秒时,SBU线被拉高,模拟引脚被短路到意外电压。当采样阶段在~49s再次发生时,我们看到SBU2线路没有与PMOS/NMOS驱动器切换,这“告诉”TPS25751已经检测到“液体”。在采样阶段结束时,液体检测信号被驱动为高电平。
很遗憾,我们没有演示代码。有关更多信息,请参阅产品页面上的EVM用户指南和技术参考手册。