ti那款芯片可以支持两节钛酸锂(2.4*2 2.8*2)电池串联 500MA充电管理?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
ti那款芯片可以支持两节钛酸锂(2.4*2 2.8*2)电池串联 500MA充电管理?
您好,
锂钛酸电池的充电曲线与锂离子电池非常相似、只是最终调节电压除外。 因此、您将需要具有反馈电阻器可调节电池稳压电压的独立充电器(例如 BQ25306)或具有 I2C 寄存器的主机控制型充电器(例如 BQ25792)。 BQ25792及其新一代 BQ25798可以实现此功能、但它们是5A 充电器、因此是通用型充电器。 在500mA 充电电流下、线性充电器可能更适合、但 TI 没有具有高达5.6V 的可调节电压的线性锂充电器。