毕业设计的时候留下了一块6V的铅蓄电池,一直放着觉得浪费,最近想着用LM22670做一块降压稳压电路给USB设备充电,结果上电的时候输出达不到设定的5V电压。我用的是LM22670-ADJ/PSOP8封装,用万用表测量FB端的电压是1.14V左右,低于规格书上面的1.285v,输出端SW的电压是4.65V左右(设定的是5V),而且波纹很大。铅蓄电池的电压是6.5V。用万用表测量输入端VIN和输出端SW的压差是1.9V。
而当我用9V的DC电源输入的时候,输出就正常了,输出电压5V,FB端电压1.285V,我的反馈电阻分别是4.3k和1.5k。
请问这是我的电路参数设置有问题吗,还是产品本身要求的输入输出压差比较高?我试了LM2596就完全可以把6.5V转化为5V输出,为什么LM22670不可以呢?