Part Number: BQ40Z80
Other Parts Discussed in Thread: BQ40Z50,
BQ40Z50 和 BQ40Z80 是否支持把采样电阻改为0.5毫欧?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
感谢您对TI产品的关注!
关于你的咨询,BQ40Z50 和 BQ40Z80 芯片通常推荐使用的采样电阻为1mohm to 3ohm,以确保测量精度和性能。
The BQ40Z80 uses the SRP and SRN inputs to measure and calculate the battery charge and discharge current
using a 1-mΩ to 3-mΩ typ. sense resistor
如果你使用0.5mohm的电阻,可能会影响电流测量的准确性和稳定性。
使用较低电阻的主要问题在于:
较小的采样电阻可能会使得测量受到更多噪声的影响。
虽然0.5毫欧的功率损耗较低,但可能不足以在特定应用中提供准确的电流采样。