This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
输入+20V以内,输出+12V以内可调,在输出+12V时电流容量在10A左右。
输入电压范围是多少?
输出电压是0~12V可调?
非常感谢您的回复:首先,最好是单路输出,输入电压为正12V,输出电压最好可设定,如设定输出3.3V、5V、12V的电压,输出电流要达到10A,求推荐DC-DC方案
HI
对于较大的输出范围,因为不同的输出,对应不同的补偿,所以你要么选择不用做外部补偿的芯片,要么选择动态补偿的数字芯片。
对于12V10A输出,推荐LM25117
对于3.3V和5V10A输出,推荐TPS53515