Other Parts Discussed in Thread: TPS54062, LM5018
如题,请求推荐一款开关电源芯片
我们只做射频模块的,我们的模块有两个MCU(CC430),有两个射频天线,两个MCU工作时功耗小于150mA;其中一个MCU的射频采用了射频增益放大器,功耗有100mA。
电源参数要求:最小输入电压范围 9~50V; 输出电压 5V
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI
TI的射频dc/dc没有供电电压到50V的,所以你还是只能选择普通的DC/DC, 例如TPS54062, 200m的同步降压DC/DC, 然后再增加以及LC,尽量把纹波和noise做到最小。
HI
DC/DC还可以选择LM5018, 如果性能要求很高,后面还可以加LDO.