你好!能推荐几款极低静态功耗的输出4.5V2A(峰值)输出DC/DC电路,由3.7V的电池通过此电路升压到4.4V为GPRS/GSM通信模块供电。
峰值拔号时,电流峰值会达2A,成本要求低。不知道,LM4000 的静态功耗是多大?
谢谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
能否具体说明一下您的输入电压范围,因为电池在供电过程中电压会下降。同时在layout空间上是否有要求,即是选择芯片内置Mos还是可以外置Mos?
可以用的芯片很多:TPS61087(75uA),TPS61030(25uA),TPS55340(500uA), TPS43000(外置MOS/1mA)
静态电流最小的是TPS61030 25uA, 输入电压范围最低的是TPS55340,最低可以到2.9V,如果可以外置MOS, TPS43000会更低,封装最小的是TPS61087 10Pin封装. 其他的都是16脚封装。
哈哈,谢谢各位,
使用3.7V锂电供电,一般低于2.7V就会保护了。输入法应在2.7V 到4V之间,对空间要求不是太严格,
谢谢,挺好的的参考资料,成本在1美元以下,最好8脚的。谢谢。