Other Parts Discussed in Thread: UC2843, TPS61175, LM2585, LM5000, TPS54360, LM2587, TPS54340
设计一个电路,需要将24V转换为正负5V,正5v负载最大1.5A,负5V负载最大1.2A,可以用两个IC完成,效率不低于80%。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
可以采用TPS54360之类降压芯片加耦合电感的设计:
http://www.ti.com.cn/cn/lit/an/slva369a/slva369a.pdf
上述文档中,可以用3.5A的TPS54360替代,设计出+/-5V/1.5A
Hi
回扫式稳压器也可以: http://www.ti.com.cn/cn/lit/ds/symlink/lm2587.pdf
参照第十四页图11,采用LM2587-5就是±/5V, 同时需要调整一下变压器匝比。