This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS6521905-Q1: TPS6521905-Q1做高低温试验,遇到-10℃后输出电压就会变成0V,此时该芯片的器件ID也无法读取

Part Number: TPS6521905-Q1


 我们的产品在做高低温试验的时候,一旦老化箱温度达到-10℃后,芯片TPS6521905-Q1的输出电压就会变成0V,此时该芯片的器件ID也无法读取(器件ID一直为0),一旦温度上升该器件输出电压就会恢复,器件ID也能读取。不知道有什么排查建议吗?

  • 感谢您对TI产品的关注!
    关于你的咨询,TPS6521905-Q1的operating temp 范围是-40 to 125度。
    你满足你的试验要求的。
    排查的话,你看看下面几点。

    1.确保TPS6521905-Q1的电源输入在-10℃时仍然正常工作。检查电源电压是否稳定,是否有低温影响电源的波动。

    2.确认芯片的输入引脚信号在-10℃时是否仍然符合工作要求。某些输入信号在低温下可能出现不稳定情况,导致芯片无法正常工作。

    3.检查PCB的设计和布局,确保没有因低温导致的物理层面问题,例如裂纹、焊接不良等,这些问题可能在温度变化时引起电路不稳定。

    4.在温度范围内尝试重启芯片,确认是否能重新恢复工作状态。这有助于确定问题是否与自复位有关。

    5.如果条件允许,可以尝试使用其他相同型号的芯片进行替代测试,以排除单个芯片的劣化或损坏。

    希望对你的问题有所帮助。