添加至 TPS61070芯片老烧 wiki 页面

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61070芯片老烧

 
原先用的3.7V电源,想升到5V,锂电池一接上去芯片温度急剧升高,立马烧坏,后来为了避免悲剧再次发生,我在连好电路之后用1.5v干电池供电,
无负载的情况下输入电流竟然还有4mA,跟说明书上写的uA级别相差甚远,在输出端量了一下电压,有4.7v,还算比较正常,然后接入100欧姆电阻当负载,
输出电流只有20mA了,再取下负载,测量输入电流,发现空载时电流竟然达到40mA了,悲剧竟然又重演了。。。。。到网上一查,发现有人有过同样经历,
问了一下说是说明书上的电路有问题,我觉得一个拿的出手的产品应该是由众多顶级工程师测试过的,说明书也应该是经过严格审阅的,应该不会有问题,
但现在问题就这样发生了,请大神来解答疑惑,(电感用的是4.7uH的色环电感,R1,R2都按照技术手册上写的)