Other Parts Discussed in Thread: TPS73801
我最近选择一款LDO芯片 输入在3.7-4.2V 输出稳定在3.3V电压 最大输出电流有1A左右 器件的漏电流小 我看上的一款电源芯片是TPS73733请问技术人员 你们觉得合适吗?? 多谢!!!!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
TPS7A733可以的,但是要注意这个芯片最大1A输出时,Vdrop的典型值是130mV,但是最大值会是500mV(应该是极端的少,但有存在可能),所以如果出现这种情况,3.7V供电是输出电压可能会偏低。
你可以选择1A时,最大Vdrop小于400mV的LDO, 例如:
TPS73801: http://www.ti.com.cn/cn/lit/ds/symlink/tps73801.pdf
TPS7A4533: http://www.ti.com.cn/product/cn/tps7a4533
等等