Part Number: TPS61130
Other Parts Discussed in Thread: TPS61299
TI技术支持您好
我现在有一个项目是用一节锂电池对整个系统供电,此前选择了TPS61130,因为它的内部集成了一个LDO。 我现在的使用需求是我需要DCDC输出一个3.3V为屏幕供电(大部分时间处于休眠状况),然后LDO输出3.3V为心电采集芯片供电,AFE的功耗大概在1mA,并且我希望整个DCDC效率越高越好请问由比TPS61130更合适的推荐吗
感谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TPS61130
Other Parts Discussed in Thread: TPS61299
TI技术支持您好
我现在有一个项目是用一节锂电池对整个系统供电,此前选择了TPS61130,因为它的内部集成了一个LDO。 我现在的使用需求是我需要DCDC输出一个3.3V为屏幕供电(大部分时间处于休眠状况),然后LDO输出3.3V为心电采集芯片供电,AFE的功耗大概在1mA,并且我希望整个DCDC效率越高越好请问由比TPS61130更合适的推荐吗
感谢
您好,
已经收到了您的案例,调查需要些时间,感谢您的耐心等待。
由于负载约为1mA、您能否试用 TPS61299、在3.3V 输出电压和2V 输入下、1mA 下的效率约为90%。
它也取决于LDO。 我只能估计提升的效率。 您可以使用升压效率乘以LDO来简单地计算总效率,然后与TPS61130进行比较。