Other Parts Discussed in Thread: UCD9244, UCD74120, UCD7242, UCD9222
我用一片UCD9244的一个PWM通道同时控制两路UCD74120,两片UCD74120的电路完全一样,然后把两片UCD74120的输出连接在一起,并联产生更大的输出电压。
两片UCD74120的FLT通过一个或门,得到一个FLT信号接到该UCD9244该通道的FLT上。
现在问题是两片UCD74120的Isenes输出,如何接到一个UCD9244通道的CSA引脚上!!
我的设计大概为如下,
原来用UCD7242时,因为UCD7242的两路Isenes输出是基于电流的,所以可以将两个Isenes一并接到UCD9222的CSA引脚上。
1. 但是,UCD74120的Isenes是基于电压的,是否应该用个电压加法器,把两片UCD74120的Isenes输出加起来,再接到UCD9244的CSA引脚?如果是这样,请推荐一个BOM最小的电压加法器。
2. 还有就是,UCD74120的Isenes可否不接到UCD9244的CS引脚上,就是不用UCD9244对UCD74120的电流进行检测。这样应该对指点电压、电流的输出没有影响吧??
在E2E发帖为e2e.ti.com/.../476520
谢谢!!!