Other Parts Discussed in Thread: TPS61088
你好:
我想请问,就是我在用TPS61088做VIN=4.2V,输出Vout=12V测试时发现当SW 在负载1.5A时尖峰电压Vp-p高达18V最后导致IC烧坏。Cout=22uF*3,并且还并联了一个1uF电容。Cin=22uF*2。布局如下:
,如果是Layout有问题或者其他方面问题,望解答,同时对于升压型转换器PCBLayout 是否有相关好的建议或者文档供学习
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: TPS61088
你好:
我想请问,就是我在用TPS61088做VIN=4.2V,输出Vout=12V测试时发现当SW 在负载1.5A时尖峰电压Vp-p高达18V最后导致IC烧坏。Cout=22uF*3,并且还并联了一个1uF电容。Cin=22uF*2。布局如下:
,如果是Layout有问题或者其他方面问题,望解答,同时对于升压型转换器PCBLayout 是否有相关好的建议或者文档供学习
你好,这用法有问题,这颗芯片不适合,SW电压最高14.5V,输出电压12V的话,很危险了,建议选择基本输出电压可以到17V的boost芯片,谢谢。
你好,你也可以把你的具体需求写出来,比如输入多少,输出多少,负载多少,让别人帮你选一下,谢谢。
你这个spec目前有很多正在是用TPS61088实现,所以只要合理设计,可以放心使用。你这边的问题出在layout上,输出电容需要横跨在在Vout和GND之间,做到输出环路极短。