实验室之前使用的是基于DM642设计的视频处理系统,使用TVP5150进行视频解码,SAA7121进行视频编码。我自行设计了基于DM648的处理系统,编解码还是用的TVP5150和SAA7121。但是实际调试发现,DM642的程序是在官方提供的DDK基础上编写的,而DM648的工程基于DVSDK,不兼容DM642的驱动程序文件。DM648的DVSDK中有TVP5154、TVP7000、SAA7105、THS8200等编解码芯片的驱动程序。
因此我想问一下,官方有没有提供DM648可以使用的TVP5150、SAA7121的驱动程序文件,还是说只能在原来的程序上修改。