MCASP里的AFIFO_WFIFOCTL、AFIFO_RFIFOCTL使能后,同时把FMT的BUSEEL设为DMA数据,产生AXEVT、AREVT事件,请问是到EDMA吗?如果是的,那么PARAM的源地址是什么呢?一直都没理解清楚,谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
是EDMA,可以参考STARTERWARE里面的代码
下面别是发送和接受的EDMA参数
static struct EDMA3CCPaRAMEntry const txDefaultPar =
{
(unsigned int)(EDMA3CC_OPT_DAM | (0x02 << 8u)), /* Opt field */
(unsigned int)loopBuf, /* source address */
(unsigned short)(BYTES_PER_SAMPLE), /* aCnt */
(unsigned short)(NUM_SAMPLES_LOOP_BUF), /* bCnt */
(unsigned int) SOC_MCASP_0_DATA_REGS, /* dest address */
(short) (BYTES_PER_SAMPLE), /* source bIdx */
(short)(0), /* dest bIdx */
(unsigned short)(PAR_TX_START * SIZE_PARAMSET), /* link address */
(unsigned short)(0), /* bCnt reload value */
(short)(0), /* source cIdx */
(short)(0), /* dest cIdx */
(unsigned short)1 /* cCnt */
};
/*
** Default paRAM for Receive section.
*/
static struct EDMA3CCPaRAMEntry const rxDefaultPar =
{
(unsigned int)(EDMA3CC_OPT_SAM | (0x02 << 8u)), /* Opt field */
(unsigned int)SOC_MCASP_0_DATA_REGS, /* source address */
(unsigned short)(BYTES_PER_SAMPLE), /* aCnt */
(unsigned short)(1), /* bCnt */
(unsigned int)rxBuf0, /* dest address */
(short) (0), /* source bIdx */
(short)(BYTES_PER_SAMPLE), /* dest bIdx */
(unsigned short)(PAR_RX_START * SIZE_PARAMSET), /* link address */
(unsigned short)(0), /* bCnt reload value */
(short)(0), /* source cIdx */
(short)(0), /* dest cIdx */
(unsigned short)1 /* cCnt */
};
请问有相关的例程么?如果有麻烦发给我学习学习,谢谢啦