你好,我这里项目由C5515升级到C5517,用的是外部IIC ROOM启动, 现在发现C5517有几点变动:
1: C5517的BOOT,现在必须由GP[26:21]6个引脚配置,C5515不需要,配置时时钟以前选择的是RTC倍频,现在发现RTC倍频改为on-chip USB oscillator,请问
on-chip USB oscillator 这个时钟是由外部提供还是内部自带的?
2:项目没有使用EMIF ,那EM_WAIT2-EM_WAIT5是否可以悬空?
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,我这里项目由C5515升级到C5517,用的是外部IIC ROOM启动, 现在发现C5517有几点变动:
1: C5517的BOOT,现在必须由GP[26:21]6个引脚配置,C5515不需要,配置时时钟以前选择的是RTC倍频,现在发现RTC倍频改为on-chip USB oscillator,请问
on-chip USB oscillator 这个时钟是由外部提供还是内部自带的?
2:项目没有使用EMIF ,那EM_WAIT2-EM_WAIT5是否可以悬空?
谢谢!
1. on-chip USB oscillator时钟有外部12M晶体提供,请参考下面的数据手册说明。
5.7.4.3.3.1 USB On-Chip Oscillator With External Crystal
http://www.ti.com/lit/ds/symlink/tms320c5517.pdf
C5515到c5517的移植文档如下。
http://www.ti.com/lit/an/sprabl8/sprabl8.pdf
2. EM_WAIT管脚内部有下拉电阻,可以悬空。