请问TMDSICE3359板子如何调试?我用的板子自带的XDS100V2好像调试不了?CCS里显示下载了但是没有反应,尝试了UART basicexample等都没有反应。还是要用starterware?starterware是用做什么的?
另,我现在想用这个板子做一个PROFINET的从机模块,要怎么做?是要把PRU-ICSS-PROFINET-SLAVE加入到sys/bios中吗?怎么加入?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
请问TMDSICE3359板子如何调试?我用的板子自带的XDS100V2好像调试不了?CCS里显示下载了但是没有反应,尝试了UART basicexample等都没有反应。还是要用starterware?starterware是用做什么的?
另,我现在想用这个板子做一个PROFINET的从机模块,要怎么做?是要把PRU-ICSS-PROFINET-SLAVE加入到sys/bios中吗?怎么加入?
1,要定位一下是XDS100V2的问题还是板子的问题。可以看看芯片能否连上,如果连上能下软件说明仿真器是好的
2,UART没有反应,看看其他DEMO能否正常,看看是否是板子硬件有问题。
3,PROFINET有专门的DEMO,把那个DEMO下载下来,按照知道文档做就可以了。
请问,GEL文件初始化时出错怎么解决?
CortxA8: Trouble Writing Memory Block at 0x4c0000e4 on Page 0 of Length 0x4: (Error -1065 @ 0x3D5A) Unable to access device memory. Verify that the memory address is in valid memory. If error persists, confirm configuration, power-cycle board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 6.0.628.3)
AM3359_ICE_Initialization() cannot be evaluated.
Target failed to write 0x4C0000E4
at *((unsigned int *) (0x4C000000+0x0E4))=(unsigned int) 0x07 [TMDXICE3359_v2_1A.gel:281]
at DDR3_EMIF_Config() [TMDXICE3359_v2_1A.gel:374]
at AM3359_ICE_Initialization()
论坛看到有人也有同样的错误,说是按照 http://processors.wiki.ti.com/index.php/AM335x_SYSBIOS_Industrial_SDK_Getting_Started_Guide#Launching_and_Debugging_application_in_CCS
擦除FLASH就可以了,但是以上链接中Flashing Binaries to SPI FLASH on ICE V1/V2 USing CCS也需要先完成GEL的AM3359_ICE_Initialization script这一步,
要怎么绕过这个GEL初始化擦除FLASH?