This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

c6678的emif nor flash启动及烧写



ti工程师您好,

 我现在需要完成自制电路板的EMIF NOR FLASH 烧写自启动,芯片是C6678,EMIF 的CE0外接一个NOR FLASH,现有如下问题,希望能得到您的解答:

1、查看其它帖子,ti工程师给出 C6678EVM板上没有EMIF 外接 NOR FLASH 所以无法使用EMIF自加载烧写NOR FLASH ,官方给出的norwrite只适用于SPI NOR 烧写,是否是这样的情况呢?

2、在6678EVM 测试,当使用EMIF 自启动时,参照手册,bootmode【12:0】=00 0000 0100 000是否正确?

3、我的参考书上给出的emif自启动nor烧写方式中,需要给原工程加入bootloade汇编文件如下:

 .ref  _c_int00
 .ref FLASH_TEXT_START
 .ref RAM_TEXT_START
 .ref TEXT_SIZE
 .ref FLASH_CINIT_START
 .ref RAM_CINIT_START
 .ref CINIT_SIZE
 .ref FLASH_CONST_START
 .ref RAM_CONST_START
 .ref CONST_SIZE
 .ref FLASH_SWITCH_START
 .ref RAM_SWITCH_START
 .ref SWITCH_SIZE
 .ref FLASH_VECT_START
 .ref RAM_VECT_START
 .ref VECT_SIZE
 .sect "bootload"

_boot_start:
  nop 5
  mvkl copyTable, a3 ;load table pointer
  mvkh copyTable, a3
copy_section_top:
 ldw *a3+ +, b0 ; byte count
 ldw *a3+ +, b4 ; load flash start (load) address
 ldw *a3+ +, a4 ; ram start address
 nop 2
 [! b0] b copy_done
 nop 5
copy_loop:
 ldb *b4+ +,b5
 sub b0,1,b0
 [ b0] b copy_loop
 [! b0] b copy_section_top
 zero a1
 [! b0] and 3,a3,a1
 stb b5,*a4+ +
 [! b0] and -4,a3,a5
 [ a1] add 4,a5,a3
copy_done:
 mvkl .S2 _c_int00, B0
 mvkh .S2 _c_int00, B0
 b .S2 B0
 nop 5
copyTable:
 ;;.text
 .word TEXT_SIZE
 .word FLASH_TEXT_START
 .word RAM_TEXT_START
 ;;.cinit
 .word CINIT_SIZE
 .word FLASH_CINIT_START
 .word RAM_CINIT_START
 ;;.const
 .word CONST_SIZE
 .word FLASH_CONST_START
 .word RAM_CONST_START
 ;;.switch
 .word SWITCH_SIZE
 .word FLASH_SWITCH_START
 .word RAM_SWITCH_START
 ;;.vect
 .word VECT_SIZE
 .word FLASH_VECT_START
 .word RAM_VECT_START
 ;;end of table
 .word 0
 .word 0
 .word 0

linker的cmd文件如下:

-c
-heap  0x4100
-stack 0xa000


MEMORY
{
 //CORE0
 L1PSRAM(RWX)  : org=0x00E00000, l=0x7FFF
 L1DSRAM(RWX)  : org=0x00F00000, l=0x7FFF
 L2SRAM(RWX)   : o = 0x00800000, l = 0x00080000
 MSMCSRAM(RWX) : o = 0x0c000000, l = 0x00200000
 DDR3(RWX)     : o = 0x80000000, l = 0x10000000
 boot          : o = 0x70000000, l = 0x00000200
 FLASH         : o = 0x70000200, l = 0x003FFE00

}

SECTIONS
{
 "bootload" :{} > boot
 .text :{}>  FLASH run = MSMCSRAM,LOAD_START(FLASH_TEXT_START),
 RUN_START(RAM_TEXT_START),SIZE(TEXT_SIZE)

 .cinit :{}> FLASH run = MSMCSRAM,LOAD_START(FLASH_CINIT_START),
 RUN_START(RAM_CINIT_START),SIZE(CINIT_SIZE)

 .const :{}> FLASH run = MSMCSRAM,LOAD_START(FLASH_CONST_START),
 RUN_START(RAM_CONST_START),SIZE(CONST_SIZE)

 .switch :{}> FLASH run = MSMCSRAM,LOAD_START(FLASH_SWITCH_START),
 RUN_START(RAM_SWITCH_START),SIZE(SWITCH_SIZE)

 .csl_vect :{}> FLASH run = MSMCSRAM,LOAD_START(FLASH_VECT_START),
 RUN_START(RAM_VECT_START),SIZE(VECT_SIZE)

 GROUP(NEAR_DP)
 {
  .neardata
  .rodata
  .bss
 }load > MSMCSRAM

 .stack  > MSMCSRAM
 .cio  > MSMCSRAM
 .data > MSMCSRAM
 .far   > MSMCSRAM
 .fardata > MSMCSRAM
 .sysmem   > MSMCSRAM
 .testMem > MSMCSRAM
}

利用工具转换成.bin文件后,利用官方给定的工具烧写(是否是指norwrite),这样操作是否正确?我该如何得知二级bootload是否进行了程序搬移?

3、如果以上均不能实现emif nor flash烧写,我该怎么操作?可否提供烧写流程及例程?十分感谢