你好,我是用335xd的核心板,你们的adc采集,AIN0-6都正常,AIN7在采集时,会偶尔出现很大的负值,而且每次都是固定值-550525552,请问可能是什么原因,要怎么排查
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
请问AIN7输入信号是正常的吗?电压是多少?
另外请贴出您使用的SDK版本以及ADC设备树部分的配置。
电压范围是正常的0-1.8V ,我不清楚sdk,而且内核是linux3.2,不是设备树的,是板级文件,下面是ti_adc.c的驱动
/* * TI ADC MFD driver * * Copyright (C) 2012 Texas Instruments Incorporated - http://www.ti.com/ * * This program is free software; you can redistribute it and/or * modify it under the terms of the GNU General Public License as * published by the Free Software Foundation version 2. * * This program is distributed "as is" WITHOUT ANY WARRANTY of any * kind, whether express or implied; without even the implied warranty * of MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the * GNU General Public License for more details. */ #include <linux/init.h> #include <linux/kernel.h> #include <linux/err.h> #include <linux/module.h> #include <linux/slab.h> #include <linux/interrupt.h> #include <linux/platform_device.h> #include <linux/io.h> #include <linux/sched.h> #include "../iio.h" #include "../sysfs.h" #include "../buffer_generic.h" #include "../ring_sw.h" #include <linux/mfd/ti_tscadc.h> #include <linux/platform_data/ti_adc.h> struct adc_device { struct ti_tscadc_dev *mfd_tscadc; struct iio_dev *idev; struct work_struct poll_work; wait_queue_head_t wq_data_avail; int channels; int irq; bool is_continuous_mode; u16 *buffer; }; static unsigned int adc_readl(struct adc_device *adc, unsigned int reg) { return readl(adc->mfd_tscadc->tscadc_base + reg); } static void adc_writel(struct adc_device *adc, unsigned int reg, unsigned int val) { writel(val, adc->mfd_tscadc->tscadc_base + reg); } static void adc_step_config(struct adc_device *adc_dev, bool mode) { unsigned int stepconfig; int i, channels = 0, steps; /* * There are 16 configurable steps and 8 analog input * lines available which are shared between Touchscreen and ADC. * * Steps backwards i.e. from 16 towards 0 are used by ADC * depending on number of input lines needed. * Channel would represent which analog input * needs to be given to ADC to digitalize data. */ steps = TOTAL_STEPS - adc_dev->channels; channels = TOTAL_CHANNELS - adc_dev->channels; if (mode == 0) stepconfig = TSCADC_STEPCONFIG_AVG_16 | TSCADC_STEPCONFIG_FIFO1; else stepconfig = TSCADC_STEPCONFIG_AVG_16 | TSCADC_STEPCONFIG_FIFO1 | TSCADC_STEPCONFIG_MODE_SWCNT; for (i = (steps + 1); i <= TOTAL_STEPS; i++) { adc_writel(adc_dev, TSCADC_REG_STEPCONFIG(i), stepconfig | TSCADC_STEPCONFIG_INP(channels)); adc_writel(adc_dev, TSCADC_REG_STEPDELAY(i), TSCADC_STEPCONFIG_OPENDLY); channels++; } } static ssize_t tiadc_show_mode(struct device *dev, struct device_attribute *attr, char *buf) { struct iio_dev *indio_dev = dev_get_drvdata(dev); struct adc_device *adc_dev = iio_priv(indio_dev); unsigned int tmp; tmp = adc_readl(adc_dev, TSCADC_REG_STEPCONFIG(TOTAL_STEPS)); tmp &= TSCADC_STEPCONFIG_MODE(1); if (tmp == 0x00) return sprintf(buf, "oneshot\n"); else if (tmp == 0x01) return sprintf(buf, "continuous\n"); else return sprintf(buf, "Operation mode unknown\n"); } static ssize_t tiadc_set_mode(struct device *dev, struct device_attribute *attr, const char *buf, size_t count) { struct iio_dev *indio_dev = dev_get_drvdata(dev); struct adc_device *adc_dev = iio_priv(indio_dev); unsigned int config; config = adc_readl(adc_dev, TSCADC_REG_CTRL); config &= ~(TSCADC_CNTRLREG_TSCSSENB); adc_writel(adc_dev, TSCADC_REG_CTRL, config); if (!strncmp(buf, "oneshot", 7)) adc_dev->is_continuous_mode = false; else if (!strncmp(buf, "continuous", 10)) adc_dev->is_continuous_mode = true; else { dev_err(dev, "Operational mode unknown\n"); return -EINVAL; } adc_step_config(adc_dev, adc_dev->is_continuous_mode); config = adc_readl(adc_dev, TSCADC_REG_CTRL); adc_writel(adc_dev, TSCADC_REG_CTRL, (config | TSCADC_CNTRLREG_TSCSSENB)); return count; } static IIO_DEVICE_ATTR(mode, S_IRUGO | S_IWUSR, tiadc_show_mode, tiadc_set_mode, 0); static struct attribute *tiadc_attributes[] = { &iio_dev_attr_mode.dev_attr.attr, NULL, }; static const struct attribute_group tiadc_attribute_group = { .attrs = tiadc_attributes, }; static irqreturn_t tiadc_irq(int irq, void *private) { struct iio_dev *idev = private; struct adc_device *adc_dev = iio_priv(idev); unsigned int status, config; status = adc_readl(adc_dev, TSCADC_REG_IRQSTATUS); if (status & TSCADC_IRQENB_FIFO1OVRRUN) { config = adc_readl(adc_dev, TSCADC_REG_CTRL); config &= ~(TSCADC_CNTRLREG_TSCSSENB); adc_writel(adc_dev, TSCADC_REG_CTRL, config); adc_writel(adc_dev, TSCADC_REG_IRQSTATUS, TSCADC_IRQENB_FIFO1OVRRUN | TSCADC_IRQENB_FIFO1UNDRFLW | TSCADC_IRQENB_FIFO1THRES); adc_writel(adc_dev, TSCADC_REG_CTRL, (config | TSCADC_CNTRLREG_TSCSSENB)); return IRQ_HANDLED; } else if (status & TSCADC_IRQENB_FIFO1THRES) { adc_writel(adc_dev, TSCADC_REG_IRQCLR, TSCADC_IRQENB_FIFO1THRES); if (iio_buffer_enabled(idev)) { if (!work_pending(&adc_dev->poll_work)) schedule_work(&adc_dev->poll_work); } else { wake_up_interruptible(&adc_dev->wq_data_avail); } return IRQ_HANDLED; } else { return IRQ_NONE; } } static void tiadc_poll_handler(struct work_struct *work_s) { struct adc_device *adc_dev = container_of(work_s, struct adc_device, poll_work); struct iio_dev *idev = iio_priv_to_dev(adc_dev); struct iio_buffer *buffer = idev->buffer; unsigned int fifo1count, readx1; int i; u32 *iBuf; fifo1count = adc_readl(adc_dev, TSCADC_REG_FIFO1CNT); if (fifo1count * sizeof(u32) < buffer->access->get_bytes_per_datum(buffer)) { dev_err(adc_dev->mfd_tscadc->dev, "%s: Short FIFO event\n", __func__); goto out; } iBuf = kmalloc(fifo1count * sizeof(u32), GFP_KERNEL); if (iBuf == NULL) goto out; for (i = 0; i < fifo1count; i++) { readx1 = adc_readl(adc_dev, TSCADC_REG_FIFO1); readx1 &= TSCADC_FIFOREAD_DATA_MASK; iBuf[i] = readx1; } buffer->access->store_to(buffer, (u8 *) iBuf, iio_get_time_ns()); kfree(iBuf); out: adc_writel(adc_dev, TSCADC_REG_IRQSTATUS, TSCADC_IRQENB_FIFO1THRES); adc_writel(adc_dev, TSCADC_REG_IRQENABLE, TSCADC_IRQENB_FIFO1THRES); } static int tiadc_buffer_preenable(struct iio_dev *idev) { struct iio_buffer *buffer = idev->buffer; buffer->access->set_bytes_per_datum(buffer, 16); return 0; } static int tiadc_buffer_postenable(struct iio_dev *idev) { struct adc_device *adc_dev = iio_priv(idev); struct iio_buffer *buffer = idev->buffer; unsigned int enb, config; int stepnum; u8 bit; if (!adc_dev->is_continuous_mode) { pr_info("Data cannot be read continuously in one shot mode\n"); return -EINVAL; } else { config = adc_readl(adc_dev, TSCADC_REG_CTRL); adc_writel(adc_dev, TSCADC_REG_CTRL, config & ~TSCADC_CNTRLREG_TSCSSENB); adc_writel(adc_dev, TSCADC_REG_CTRL, config | TSCADC_CNTRLREG_TSCSSENB); adc_writel(adc_dev, TSCADC_REG_IRQSTATUS, TSCADC_IRQENB_FIFO1THRES | TSCADC_IRQENB_FIFO1OVRRUN | TSCADC_IRQENB_FIFO1UNDRFLW); adc_writel(adc_dev, TSCADC_REG_IRQENABLE, TSCADC_IRQENB_FIFO1THRES | TSCADC_IRQENB_FIFO1OVRRUN); adc_writel(adc_dev, TSCADC_REG_SE, 0x00); for_each_set_bit(bit, buffer->scan_mask, adc_dev->channels) { struct iio_chan_spec const *chan = idev->channels + bit; /* * There are a total of 16 steps available * that are shared between ADC and touchscreen. * We start configuring from step 16 to 0 incase of * ADC. Hence the relation between input channel * and step for ADC would be as below. */ stepnum = chan->channel + 9; enb = adc_readl(adc_dev, TSCADC_REG_SE); enb |= (1 << stepnum); adc_writel(adc_dev, TSCADC_REG_SE, enb); } return 0; } } static int tiadc_buffer_postdisable(struct iio_dev *idev) { struct adc_device *adc_dev = iio_priv(idev); adc_writel(adc_dev, TSCADC_REG_IRQCLR, (TSCADC_IRQENB_FIFO1THRES | TSCADC_IRQENB_FIFO1OVRRUN | TSCADC_IRQENB_FIFO1UNDRFLW)); adc_writel(adc_dev, TSCADC_REG_SE, TSCADC_STPENB_STEPENB_TC); return 0; } static const struct iio_buffer_setup_ops tiadc_swring_setup_ops = { .preenable = &tiadc_buffer_preenable, .postenable = &tiadc_buffer_postenable, .postdisable = &tiadc_buffer_postdisable, }; static int tiadc_config_sw_ring(struct iio_dev *idev) { struct adc_device *adc_dev = iio_priv(idev); int ret; idev->buffer = iio_sw_rb_allocate(idev); if (!idev->buffer) ret = -ENOMEM; idev->buffer->access = &ring_sw_access_funcs; idev->buffer->setup_ops = &tiadc_swring_setup_ops; INIT_WORK(&adc_dev->poll_work, &tiadc_poll_handler); idev->modes |= INDIO_BUFFER_HARDWARE; return 0; } static int tiadc_channel_init(struct iio_dev *idev, struct adc_device *adc_dev) { struct iio_chan_spec *chan_array; int i, channels; idev->num_channels = adc_dev->channels; chan_array = kcalloc(idev->num_channels, sizeof(struct iio_chan_spec), GFP_KERNEL); if (chan_array == NULL) return -ENOMEM; channels = TOTAL_CHANNELS - adc_dev->channels; for (i = 0; i < (idev->num_channels); i++) { struct iio_chan_spec *chan = chan_array + i; chan->type = IIO_VOLTAGE; chan->indexed = 1; chan->channel = channels; chan->scan_index = i; chan->scan_type.sign = 'u'; chan->scan_type.realbits = 12; chan->scan_type.storagebits = 32; chan->scan_type.shift = 0; channels++; } idev->channels = chan_array; return idev->num_channels; } static void tiadc_channel_remove(struct iio_dev *idev) { kfree(idev->channels); } static int tiadc_read_raw(struct iio_dev *idev, struct iio_chan_spec const *chan, int *val, int *val2, long mask) { struct adc_device *adc_dev = iio_priv(idev); int i, map_val, tmp; unsigned int fifo1count, readx1, stepid; unsigned long timeout = jiffies + usecs_to_jiffies (IDLE_TIMEOUT * adc_dev->channels); if (adc_dev->is_continuous_mode) { pr_info("One shot mode not enabled\n"); return -EINVAL; } else { if(adc_dev->channels == 4) tmp = (1 << (chan->channel + TOTAL_CHANNELS + 1)) | TSCADC_STPENB_STEPENB_TC; else tmp = (1 << (chan->channel + TOTAL_CHANNELS + 1)); adc_writel(adc_dev, TSCADC_REG_SE, tmp); /* Wait for ADC sequencer to complete sampling */ while (adc_readl(adc_dev, TSCADC_REG_ADCFSM) & TSCADC_SEQ_STATUS) { if (time_after(jiffies, timeout)) return -EAGAIN; } map_val = chan->channel + TOTAL_CHANNELS; *val = -1; timeout = jiffies + usecs_to_jiffies (IDLE_TIMEOUT * adc_dev->channels); while(1){ fifo1count = adc_readl(adc_dev, TSCADC_REG_FIFO1CNT); if(!fifo1count){ if (time_after(jiffies, timeout)){ printk("wait fifo timeout\n"); return -EAGAIN; } else continue; } for (i = 0; i < fifo1count; i++) { readx1 = adc_readl(adc_dev, TSCADC_REG_FIFO1); stepid = readx1 & TSCADC_FIFOREAD_CHNLID_MASK; stepid = stepid >> 0x10; if (stepid == map_val) { readx1 = readx1 & TSCADC_FIFOREAD_DATA_MASK; *val = readx1; } } if(*val != -1){ break; } } return IIO_VAL_INT; } } static const struct iio_info tiadc_info = { .read_raw = &tiadc_read_raw, .attrs = &tiadc_attribute_group, }; static int __devinit tiadc_probe(struct platform_device *pdev) { struct iio_dev *idev; struct adc_device *adc_dev = NULL; struct ti_tscadc_dev *tscadc_dev = pdev->dev.platform_data; struct mfd_tscadc_board *pdata; int err; pdata = (struct mfd_tscadc_board *)tscadc_dev->dev->platform_data; if (!pdata || !pdata->adc_init) { dev_err(tscadc_dev->dev, "Could not find platform data\n"); return -EINVAL; } idev = iio_allocate_device(sizeof(struct adc_device)); if (idev == NULL) { dev_err(&pdev->dev, "failed to allocate iio device.\n"); err = -ENOMEM; goto err_ret; } adc_dev = iio_priv(idev); tscadc_dev->adc = adc_dev; adc_dev->mfd_tscadc = tscadc_dev; adc_dev->idev = idev; adc_dev->channels = pdata->adc_init->adc_channels; adc_dev->irq = tscadc_dev->irq; idev->dev.parent = &pdev->dev; idev->name = dev_name(&pdev->dev); idev->modes = INDIO_DIRECT_MODE; idev->info = &tiadc_info; /* by default driver comes up with oneshot mode */ adc_step_config(adc_dev, adc_dev->is_continuous_mode); /* program FIFO threshold to value minus 1 */ adc_writel(adc_dev, TSCADC_REG_FIFO1THR, FIFO1_THRESHOLD); err = tiadc_channel_init(idev, adc_dev); if (err < 0) goto err_free_device; init_waitqueue_head(&adc_dev->wq_data_avail); err = request_irq(adc_dev->irq, tiadc_irq, IRQF_SHARED, idev->name, idev); if (err) goto err_cleanup_channels; err = tiadc_config_sw_ring(idev); if (err) goto err_free_irq; err = iio_buffer_register(idev, idev->channels, idev->num_channels); if (err < 0) goto err_free_sw_rb; err = iio_device_register(idev); if (err) goto err_unregister; dev_info(&pdev->dev, "attached adc driver\n"); platform_set_drvdata(pdev, idev); return 0; err_unregister: iio_buffer_unregister(idev); err_free_sw_rb: iio_sw_rb_free(idev->buffer); err_free_irq: free_irq(adc_dev->irq, idev); err_cleanup_channels: tiadc_channel_remove(idev); err_free_device: iio_free_device(idev); err_ret: return err; } static int __devexit tiadc_remove(struct platform_device *pdev) { struct ti_tscadc_dev *tscadc_dev = pdev->dev.platform_data; struct adc_device *adc_dev = tscadc_dev->adc; struct iio_dev *idev = adc_dev->idev; free_irq(adc_dev->irq, idev); iio_device_unregister(idev); iio_buffer_unregister(idev); iio_sw_rb_free(idev->buffer); tiadc_channel_remove(idev); tscadc_dev->adc = NULL; iio_free_device(idev); platform_set_drvdata(pdev, NULL); return 0; } static int adc_suspend(struct platform_device *pdev, pm_message_t state) { struct ti_tscadc_dev *tscadc_dev = pdev->dev.platform_data; struct adc_device *adc_dev = tscadc_dev->adc; unsigned int idle; if (!device_may_wakeup(tscadc_dev->dev)) { idle = adc_readl(adc_dev, TSCADC_REG_CTRL); idle &= ~(TSCADC_CNTRLREG_TSCSSENB); adc_writel(adc_dev, TSCADC_REG_CTRL, (idle | TSCADC_CNTRLREG_POWERDOWN)); } return 0; } static int adc_resume(struct platform_device *pdev) { struct ti_tscadc_dev *tscadc_dev = pdev->dev.platform_data; struct adc_device *adc_dev = tscadc_dev->adc; unsigned int restore; restore = adc_readl(adc_dev, TSCADC_REG_CTRL); restore &= ~(TSCADC_CNTRLREG_TSCSSENB); adc_writel(adc_dev, TSCADC_REG_CTRL, restore); adc_writel(adc_dev, TSCADC_REG_FIFO1THR, FIFO1_THRESHOLD); adc_step_config(adc_dev, adc_dev->is_continuous_mode); /* Make sure ADC is powered up */ restore &= ~(TSCADC_CNTRLREG_POWERDOWN); restore |= TSCADC_CNTRLREG_TSCSSENB; adc_writel(adc_dev, TSCADC_REG_CTRL, restore); return 0; } static struct platform_driver tiadc_driver = { .driver = { .name = "tiadc", .owner = THIS_MODULE, }, .probe = tiadc_probe, .remove = __devexit_p(tiadc_remove), .suspend = adc_suspend, .resume = adc_resume, }; module_platform_driver(tiadc_driver); MODULE_DESCRIPTION("TI ADC controller driver"); MODULE_AUTHOR("Rachna Patil <rachna@ti.com>"); MODULE_LICENSE("GPL");
Linux 内核 3.2 太旧,我们无法支持。该版本的ADC 驱动程序和 Linux 5.4 之间有很多变化(肯定的是在驱动程序的触摸屏部分有变化,不确定 tscadc 驱动程序的其他部分)。如果您可以在 Linux Processor SDK 6.3 或 Linux Processor SDK 7.3 上复现问题,我们将能够提供更好的支持。
另外请问该现象是在一块板子上出现的还是多块板子?