[ 0.000000] ------------[ cut here ]------------
[ 0.000000] WARNING: at arch/arm/mach-omap2/pm.c:94 _init_omap_device+0x84/0xa4()
[ 0.000000] _init_omap_device: could not find omap_hwmod for iva
[ 0.000000] Modules linked in:
[ 0.000000] [<c00a3678>] (unwind_backtrace+0x0/0xec) from [<c00c7924>] (warn_slowpath_common+0x4c/0x64)
[ 0.000000] [<c00c7924>] (warn_slowpath_common+0x4c/0x64) from [<c00c79bc>] (warn_slowpath_fmt+0x2c/0x3c)
[ 0.000000] [<c00c79bc>] (warn_slowpath_fmt+0x2c/0x3c) from [<c00aad54>] (_init_omap_device+0x84/0xa4)
[ 0.000000] [<c00aad54>] (_init_omap_device+0x84/0xa4) from [<c000fda8>] (omap2_common_pm_init+0x2c/0x10c)
[ 0.000000] [<c000fda8>] (omap2_common_pm_init+0x2c/0x10c) from [<c00933b8>] (do_one_initcall+0xc8/0x1a0)
[ 0.000000] [<c00933b8>] (do_one_initcall+0xc8/0x1a0) from [<c0008690>] (kernel_init+0x94/0x14c)
[ 0.000000] [<c0008690>] (kernel_init+0x94/0x14c) from [<c009e590>] (kernel_thread_exit+0x0/0x8)
[ 0.000000] ---[ end trace 1b75b31a2719ed1c ]---
我有时候系统会死机,这个警告要怎么消除 谢谢 还有我用的是AM3505