1. 在存储器性能测试文档里,L2cache是否开启及开启的大小情况下,对外部内存读写的差别有点大,开启L2cache时,从l2到外部ram的速度比较低,从外部ram到l2比较快。速度差别主要是因为什么原因?
2. l2 cache在32k,64k,128k到256k情况下,cold cache测试时,L2和外部存储器相互读写速度的差别有多大?在ccs中进行ETB调试能够实时跟踪记录cache使用情况?
3. 多核使用同一个工程时,对没有进行启动的内核的L1,L2内存能否作为普通共享ram,在platform及cmd文件里配置,给其他核使用?