我所使用的DM368的板子上音频编解码芯片是tlv320aic3101,现在要求实现音频输入输出功能,不知道要如何来实现,或者是说如何来驱动tlv320aic3101?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我所使用的DM368的板子上音频编解码芯片是tlv320aic3101,现在要求实现音频输入输出功能,不知道要如何来实现,或者是说如何来驱动tlv320aic3101?
http://support.spectrumdigital.com/boards/evmdm365/revf/
原理图看这里
额你是要找驱动是吧。看这里
http://www.ti.com.cn/tool/cn/linuxdvsdk-dm36x
其实不是一定要驱动,我这个板子有一套现成的内核,现在主要不知道内核配置里该如何配置,按默认的内核配置,板子没法实现声音输入输出的,所以可能需要修改sound card support的内核配置。但是现在不知道该如何配置。另外,个人认为根据板上的音频芯片,在DM365 codec select选项里是不是应该选则Audio Codec AIC3101,原来默认的是选Voice Codec CQ93VC.但是我只改变这个选项的话,启动内核时会出现如下错误:
ALSA lib confmisc.c:768:(parse_card) cannot find card '0'
ALSA lib conf.c:4184:(_snd_config_evaluate) function snd_func_card_driver returned error: No such file or directory
ALSA lib confmisc.c:392:(snd_func_concat) error evaluating strings
ALSA lib conf.c:4184:(_snd_config_evaluate) function snd_func_concat returned error: No such file or directory
ALSA lib confmisc.c:1251:(snd_func_refer) error evaluating name
ALSA lib conf.c:4184:(_snd_config_evaluate) function snd_func_refer returned error: No such file or directory
ALSA lib conf.c:4663:(snd_config_expand) Evaluate error: No such file or directory
ALSA lib pcm.c:2212:(snd_pcm_open_noupdate) Unknown PCM [ 6.666688] Loading iSCSI transport class v2.0-870.
default
本人 比较菜,弄了好多天都不知道该如何解决,还望指教!
不知道该看那个,而且这些太宽泛了,可能不适合我的问题,求直解!