This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

am335x板子不能从nand启动以及AM335x Nand 启动UBI出错----请大牛们帮忙分析一下

Other Parts Discussed in Thread: AM3352, TPS65217

我就是按着这个这篇文档制作ubifs的,到最后依然没有能加载ubifs。

简单描述一下我的情况:我们的板子是参考BBB做的,但没有eeprom,板子没有eMMC,而是用的nand flash,除此之外和BBB没多大区别了,现在用的这款主芯片是AM3352。在uboot中改了iic读取eeprom部分,改成BBB的信息,让内核以为是BBB,然后启动。用的SDK包是SDK6.0,内核是3.2,uboot是2013.01.01版本。目前做的SD卡启动,完全没有问题,uboot、kernel和文件系统都没有问题,能启动正常。

遇到了两个问题:

1. SD卡启动uboot后,把MLO, u-boot.img, uImage, ubi,img烧写到板子的nand里,然后上电后,串口打印一直是CCC,并没有从nand启动,板子的SYSBOOT[4:0]=10011b,按说启动顺序是NAND-NANDI2C-MMC-UART,应该从nand启动的,但是没有,具体nandflash型号为:S34ML01G100TF100 。

2.从SD卡启动uboot后,烧写上面那些文件后,拔掉SD卡,输入boot命令,会从nand读取内核,并启动,但是到了要打开ubi0:rootfs的时候出错了,详细的启动打印信息在下面:

请各位前辈和TI的工程师,帮忙分析一下问题可能出在哪里,试了很多方法都不行,这里先谢谢各位大牛了。

U-Boot 2013.01.01 (Oct 24 2014 - 16:56:28)

I2C: ready
DRAM: 256 MiB
WARNING: Caches not enabled
SKW board, run without EEPROM!
SKW board use default setting as BBB
board header name: [A335BNLT0A5C3513BBBK2751]
board header version: [0A5C3513BBBK2751]
board header serial: [3513BBBK2751]
NAND: 128 MiB
MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1
*** Warning - bad CRC, using default environment

musb-hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, bulk combine, bulk split, HB-ISO Rx, HB-ISO Tx, SoftConn)
musb-hdrc: MHDRC RTL version 2.0
musb-hdrc: setup fifo_mode 4
musb-hdrc: 28/31 max ep, 16384/16384 memory
USB Peripheral mode controller at 47401000 using PIO, IRQ 0
musb-hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, bulk combine, bulk split, HB-ISO Rx, HB-ISO Tx, SoftConn)
musb-hdrc: MHDRC RTL version 2.0
musb-hdrc: setup fifo_mode 4
musb-hdrc: 28/31 max ep, 16384/16384 memory
USB Host mode controller at 47401800 using PIO, IRQ 0
Net: <ethaddr> not set. Validating first E-fuse MAC
PHY reset timed out
cpsw, usb_ether
Hit any key to stop autoboot: 0

U-Boot# boot
Card did not respond to voltage select!
mmc0(part 0) is current device
Card did not respond to voltage select!
Booting from nand ...

NAND read: device 0 offset 0x280000, size 0x600000
6291456 bytes read: OK
## Booting kernel from Legacy Image at 80200000 ...
Image Name: Linux-3.2.0
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 3249840 Bytes = 3.1 MiB
Load Address: 80008000
Entry Point: 80008000
Verifying Checksum ... OK
Loading Kernel Image ... OK
OK

Starting kernel ...

Uncompressing Linux... done, booting the kernel.
[ 0.000000] Linux version 3.2.0 (linux@ubuntu) (gcc version 4.8.3 20140303 (prerelease) (crosstool-NG linaro-1.13.1-4.8-2014.03 - Linaro GCC 2014.03) ) #3 Mon Oct 27 14:31:32 CST 2014
[ 0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c53c7d
[ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
[ 0.000000] Machine: am335xevm
[ 0.000000] Memory policy: ECC disabled, Data cache writeback
[ 0.000000] AM335X ES1.0 (neon )
[ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pages: 65024
[ 0.000000] Kernel command line: console=ttyO0,115200n8 root=ubi0:rootfs rw ubi.mtd=7,2048 rootfstype=ubifs rootwait=1
[ 0.000000] PID hash table entries: 1024 (order: 0, 4096 bytes)
[ 0.000000] Dentry cache hash table entries: 32768 (order: 5, 131072 bytes)
[ 0.000000] Inode-cache hash table entries: 16384 (order: 4, 65536 bytes)
[ 0.000000] Memory: 256MB = 256MB total
[ 0.000000] Memory: 252856k/252856k available, 9288k reserved, 0K highmem
[ 0.000000] Virtual kernel memory layout:
[ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB)
[ 0.000000] fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)
[ 0.000000] vmalloc : 0xd0800000 - 0xff000000 ( 744 MB)
[ 0.000000] lowmem : 0xc0000000 - 0xd0000000 ( 256 MB)
[ 0.000000] modules : 0xbf000000 - 0xc0000000 ( 16 MB)
[ 0.000000] .text : 0xc0008000 - 0xc05a6000 (5752 kB)
[ 0.000000] .init : 0xc05a6000 - 0xc063e000 ( 608 kB)
[ 0.000000] .data : 0xc063e000 - 0xc06a7070 ( 421 kB)
[ 0.000000] .bss : 0xc06a7094 - 0xc06d5e64 ( 188 kB)
[ 0.000000] NR_IRQS:396
[ 0.000000] IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts
[ 0.000000] Total of 128 interrupts on 1 active controller
[ 0.000000] OMAP clockevent source: GPTIMER2 at 24000000 Hz
[ 0.000000] OMAP clocksource: GPTIMER1 at 32768 Hz
[ 0.000000] sched_clock: 32 bits at 32kHz, resolution 30517ns, wraps every 131071999ms
[ 0.000000] Console: colour dummy device 80x30
[ 0.000274] Calibrating delay loop... 298.59 BogoMIPS (lpj=1492992)
[ 0.067657] pid_max: default: 32768 minimum: 301
[ 0.067932] Security Framework initialized
[ 0.068084] Mount-cache hash table entries: 512
[ 0.068756] CPU: Testing write buffer coherency: ok
[ 0.093780] omap_hwmod: gfx: failed to hardreset
[ 0.111785] omap_hwmod: pruss: failed to hardreset
[ 0.113708] print_constraints: dummy:
[ 0.114440] NET: Registered protocol family 16
[ 0.118713] OMAP GPIO hardware version 0.1
[ 0.124237] omap_mux_init: Add partition: #1: core, flags: 0
[ 0.127929] +++++++++yidaji++++++++++
[ 0.128021] omap_i2c.1: alias fck already exists
[ 0.128448] ---------yidaji----------
[ 0.128570]
[ 0.128570]
[ 0.128570]
[ 0.128601] i2c1_init_szr has been executed
[ 0.128601]
[ 0.128601]
[ 0.128631]
[ 0.128997] omap_i2c.2: alias fck already exists
[ 0.129425]
[ 0.129455]
[ 0.129455] omap_register_i2c1_bus has succeed
[ 0.129486]
[ 0.129486]
[ 0.130279] +++++++++++++naloudou+++++++++++++++++++
[ 0.130950] omap2_mcspi.1: alias fck already exists
[ 0.131439] omap2_mcspi.2: alias fck already exists
[ 0.133453] edma.0: alias fck already exists
[ 0.133483] edma.0: alias fck already exists
[ 0.133544] edma.0: alias fck already exists
[ 0.193817] bio: create slab <bio-0> at 0
[ 0.198425] SCSI subsystem initialized
[ 0.201690] usbcore: registered new interface driver usbfs
[ 0.202362] usbcore: registered new interface driver hub
[ 0.202758] usbcore: registered new device driver usb
[ 0.203308] registerd cppi-dma Intr @ IRQ 17
[ 0.203338] Cppi41 Init Done Qmgr-base(d087a000) dma-base(d0878000)
[ 0.203369] Cppi41 Init Done
[ 0.203399] musb-ti81xx musb-ti81xx: musb0, board_mode=0x13, plat_mode=0x3
[ 0.204010] musb-ti81xx musb-ti81xx: musb1, board_mode=0x13, plat_mode=0x1
[ 0.206420] omap_i2c omap_i2c.1: bus 1 rev2.4.0 at 100 kHz
[ 0.209411] tps65910 1-002d: could not be detected

[ 0.227752] omap_i2c omap_i2c.2: bus 2 rev2.4.0 at 100 kHz

[ 0.231079] Advanced Linux Sound Architecture Driver Version 1.0.24.
[ 0.233337] Switching to clocksource gp timer
[ 0.267974] musb-hdrc: version 6.0, ?dma?, otg (peripheral+host)
[ 0.268280] musb-hdrc musb-hdrc.0: dma type: dma-cppi41
[ 0.268890] MUSB0 controller's USBSS revision = 4ea20800
[ 0.270874] musb-hdrc musb-hdrc.0: USB OTG mode controller at d083c000 using DMA, IRQ 18
[ 0.271179] musb-hdrc musb-hdrc.1: dma type: dma-cppi41
[ 0.271789] MUSB1 controller's USBSS revision = 4ea20800
[ 0.272735] musb-hdrc musb-hdrc.1: MUSB HDRC host driver
[ 0.272888] musb-hdrc musb-hdrc.1: new USB bus registered, assigned bus number 1
[ 0.273101] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
[ 0.273162] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 0.273193] usb usb1: Product: MUSB HDRC host driver
[ 0.273223] usb usb1: Manufacturer: Linux 3.2.0 musb-hcd
[ 0.273223] usb usb1: SerialNumber: musb-hdrc.1
[ 0.275085] hub 1-0:1.0: USB hub found
[ 0.275146] hub 1-0:1.0: 1 port detected
[ 0.276214] musb-hdrc musb-hdrc.1: USB Host mode controller at d083e800 using DMA, IRQ 19
[ 0.276977] NET: Registered protocol family 2
[ 0.277313] IP route cache hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.277862] TCP established hash table entries: 8192 (order: 4, 65536 bytes)
[ 0.278228] TCP bind hash table entries: 8192 (order: 3, 32768 bytes)
[ 0.278472] TCP: Hash tables configured (established 8192 bind 8192)
[ 0.278503] TCP reno registered
[ 0.278533] UDP hash table entries: 256 (order: 0, 4096 bytes)
[ 0.278564] UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
[ 0.278991] NET: Registered protocol family 1
[ 0.279479] RPC: Registered named UNIX socket transport module.
[ 0.279510] RPC: Registered udp transport module.
[ 0.279510] RPC: Registered tcp transport module.
[ 0.279541] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.279968] NetWinder Floating Point Emulator V0.97 (double precision)
[ 0.295532] VFS: Disk quotas dquot_6.5.2
[ 0.295654] Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
[ 0.296691] msgmni has been set to 493
[ 0.302795] alg: No test for stdrng (krng)
[ 0.304016] io scheduler noop registered
[ 0.304046] io scheduler deadline registered
[ 0.304168] io scheduler cfq registered (default)
[ 0.306274] Could not set LED4 to fully on
[ 0.309295] omap_uart.0: ttyO0 at MMIO 0x44e09000 (irq = 72) is a OMAP UART0
[ 0.932220] ti81xx_interrupt 1146: VBUS error workaround (delay coming)
[ 0.939208] console [ttyO0] enabled
[ 0.944030] omap_uart.1: ttyO1 at MMIO 0x48022000 (irq = 73) is a OMAP UART1
[ 0.952301] omap_uart.2: ttyO2 at MMIO 0x48024000 (irq = 74) is a OMAP UART2
[ 0.960510] omap_uart.3: ttyO3 at MMIO 0x481a6000 (irq = 44) is a OMAP UART3
[ 0.968750] omap_uart.4: ttyO4 at MMIO 0x481a8000 (irq = 45) is a OMAP UART4
[ 0.977020] omap_uart.5: ttyO5 at MMIO 0x481aa000 (irq = 46) is a OMAP UART5
[ 0.986267] omap4_rng omap4_rng: OMAP4 Random Number Generator ver. 2.00
[ 1.013610] brd: module loaded
[ 1.027832] loop: module loaded
[ 1.031494] i2c-core: driver [tsl2550] using legacy suspend method
[ 1.038024] i2c-core: driver [tsl2550] using legacy resume method
[ 1.044555] at24 1-0051: 32768 byte 24c256 EEPROM, writable, 64 bytes/write
[ 1.103942] No daughter card found
[ 1.107604] at24 1-0050: 32768 byte 24c256 EEPROM, writable, 64 bytes/write
[ 1.114898] The board is a AM335x Beaglebone Black.
[ 1.122955] tps65217 1-0024: TPS65217 ID 0xe version 1.2
[ 1.131347] print_constraints: DCDC1: 900 <--> 1800 mV at 1500 mV
[ 1.140716] print_constraints: DCDC2: 900 <--> 3300 mV at 1125 mV
[ 1.149993] print_constraints: DCDC3: 900 <--> 1500 mV at 1125 mV
[ 1.159271] print_constraints: LDO1: 1000 <--> 3300 mV at 1800 mV
[ 1.168548] print_constraints: LDO2: 900 <--> 3300 mV at 3300 mV
[ 1.177734] print_constraints: LDO3: 1800 <--> 3300 mV at 1800 mV
[ 1.187072] print_constraints: LDO4: 1800 <--> 3300 mV at 3300 mV
[ 1.195007] omap_hsmmc.0: alias fck already exists
[ 1.200805] omap_hsmmc.1: alias fck already exists
[ 1.206573]
[ 1.208129]
[ 1.209686]
[ 1.211273] i2c1_init has been executed
[ 1.215332]
[ 1.216888]
[ 1.218444]
[ 1.220123] omap_i2c.3: alias fck already exists
[ 1.225738] omap_i2c omap_i2c.3: bus 3 rev2.4.0 at 100 kHz
[ 1.232849] da8xx_lcdc.0: alias fck already exists
[ 1.238739] da8xx_lcdc da8xx_lcdc.0: GLCD: Found INNOLUX_TN92 panel
[ 1.265106] Console: switching to colour frame buffer device 100x30
[ 1.295410] _omap_mux_get_by_name: Could not find signal ain0.ain0
[ 1.301940] _omap_mux_get_by_name: Could not find signal ain1.ain1
[ 1.308471] _omap_mux_get_by_name: Could not find signal ain2.ain2
[ 1.314971] _omap_mux_get_by_name: Could not find signal ain3.ain3
[ 1.321472] _omap_mux_get_by_name: Could not find signal vrefp.vrefp
[ 1.328155] _omap_mux_get_by_name: Could not find signal vrefn.vrefn
[ 1.337097] omap-gpmc omap-gpmc: GPMC revision 6.0
[ 1.342132] Registering NAND on CS0
[ 1.354309] mtdoops: mtd device (mtddev=name/number) must be supplied
[ 1.362030] omap2-nand driver initializing
[ 1.366821] ONFI flash detected
[ 1.370269] ONFI param page 0 valid
[ 1.373962] NAND device: Manufacturer ID: 0x01, Chip ID: 0xf1 (AMD S34ML01G1)
[ 1.381805] Creating 8 MTD partitions on "omap2-nand.0":
[ 1.387451] 0x000000000000-0x000000020000 : "SPL"
[ 1.395416] 0x000000020000-0x000000040000 : "SPL.backup1"
[ 1.403808] 0x000000040000-0x000000060000 : "SPL.backup2"
[ 1.412048] 0x000000060000-0x000000080000 : "SPL.backup3"
[ 1.420349] 0x000000080000-0x000000260000 : "U-Boot"
[ 1.428924] 0x000000260000-0x000000280000 : "U-Boot Env"
[ 1.437225] 0x000000280000-0x000000780000 : "Kernel"
[ 1.447235] 0x000000780000-0x000008000000 : "File System"
[ 1.507507] OneNAND driver initializing
[ 1.512939] UBI: attaching mtd7 to ubi0
[ 1.517059] UBI: physical eraseblock size: 131072 bytes (128 KiB)
[ 1.523620] UBI: logical eraseblock size: 126976 bytes
[ 1.529296] UBI: smallest flash I/O unit: 2048
[ 1.534271] UBI: VID header offset: 2048 (aligned 2048)
[ 1.540557] UBI: data offset: 4096
[ 2.622680] UBI: max. sequence number: 0
[ 2.639221] UBI error: vtbl_check: volume table check failed: record 0, error 9
[ 2.647613] UBI error: ubi_init: cannot attach mtd7
[ 2.654602] CAN device driver interface
[ 2.658630] CAN bus driver for Bosch D_CAN controller 1.0
[ 2.714080] davinci_mdio davinci_mdio.0: davinci mdio revision 1.6
[ 2.720550] davinci_mdio davinci_mdio.0: detected phy mask fffffffb
[ 2.728271] davinci_mdio.0: probed
[ 2.731872] davinci_mdio davinci_mdio.0: phy[2]: device 0:02, driver SMSC LAN8710/LAN8720
[ 2.741210] usbcore: registered new interface driver zd1201
[ 2.747467] usbcore: registered new interface driver cdc_ether
[ 2.753936] usbcore: registered new interface driver cdc_eem
[ 2.760253] usbcore: registered new interface driver dm9601
[ 2.766204] cdc_ncm: 04-Aug-2011
[ 2.769958] usbcore: registered new interface driver cdc_ncm
[ 2.775939] Initializing USB Mass Storage driver...
[ 2.781524] usbcore: registered new interface driver usb-storage
[ 2.787841] USB Mass Storage support registered.
[ 2.793670] mousedev: PS/2 mouse device common for all mice
[ 2.801544] input: ti-tsc as /devices/platform/omap/ti_tscadc/tsc/input/input0
[ 2.811279] omap_rtc am33xx-rtc: rtc core: registered am33xx-rtc as rtc0
[ 2.818695] i2c /dev entries driver
[ 2.824127] Linux video capture interface: v2.00
[ 2.829681] usbcore: registered new interface driver uvcvideo
[ 2.835723] USB Video Class driver (1.1.1)
[ 2.924041] ti81xx_interrupt 1146: VBUS error workaround (delay coming)
[ 3.864013] omap_i2c omap_i2c.2: timeout waiting for bus ready
[ 4.884033] omap_i2c omap_i2c.2: timeout waiting for bus ready
[ 5.904022] omap_i2c omap_i2c.2: timeout waiting for bus ready
[ 6.924041] omap_i2c omap_i2c.2: timeout waiting for bus ready
[ 7.944030] omap_i2c omap_i2c.2: timeout waiting for bus ready
[ 8.964019] omap_i2c omap_i2c.2: timeout waiting for bus ready
[ 9.984039] omap_i2c omap_i2c.2: timeout waiting for bus ready
[ 11.004028] omap_i2c omap_i2c.2: timeout waiting for bus ready
[ 11.012695] OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec
[ 11.096099] cpuidle: using governor ladder
[ 11.101104] cpuidle: using governor menu
[ 11.109466] omap4_aes_mod_init: loading AM33X AES driver
[ 11.115234] omap4-aes omap4-aes: AM33X AES hw accel rev: 3.02
[ 11.121917] omap4_aes_probe: probe() done
[ 11.126739] omap4_sham_mod_init: loading AM33X SHA/MD5 driver
[ 11.132934] omap4-sham omap4-sham: AM33X SHA/MD5 hw accel rev: 4.03
[ 11.149383] omap4_sham_probe: probe() done
[ 11.158477] usbcore: registered new interface driver usbhid
[ 11.164398] usbhid: USB HID core driver
[ 11.169250] tiadc tiadc: attached adc driver
[ 11.174682] usbcore: registered new interface driver snd-usb-audio
[ 11.183349] ALSA device list:
[ 11.186523] No soundcards found.
[ 11.190093] oprofile: hardware counters not available
[ 11.195434] oprofile: using timer interrupt.
[ 11.199981] nf_conntrack version 0.5.0 (3950 buckets, 15800 max)
[ 11.206909] ip_tables: (C) 2000-2006 Netfilter Core Team
[ 11.212646] TCP cubic registered
[ 11.216094] NET: Registered protocol family 17
[ 11.220794] can: controller area network core (rev 20090105 abi 8)
[ 11.227447] NET: Registered protocol family 29
[ 11.232116] can: raw protocol (rev 20090105)
[ 11.236633] can: broadcast manager protocol (rev 20090105 t)
[ 11.242645] Registering the dns_resolver key type
[ 11.247711] VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3
[ 11.255828] ThumbEE CPU extension supported.
[ 11.260406] mux: Failed to setup hwmod io irq -22
[ 11.266204] Power Management for AM33XX family
[ 11.271118] Trying to load am335x-pm-firmware.bin (60 secs timeout)
[ 11.277893] Copied the M3 firmware to UMEM
[ 11.282287] Cortex M3 Firmware Version = 0x181
[ 11.287719] sr_init: platform driver register failed
[ 11.297302] clock: disabling unused clocks to save power
[ 11.319763] Detected MACID=34:b1:f7:1a:1d:93
[ 11.325683] cpsw: Detected MACID = 34:b1:f7:1a:1d:94
[ 11.332305] omap_rtc am33xx-rtc: setting system clock to 2000-01-01 00:00:08 UTC (946684808)
[ 11.341735] VFS: Cannot open root device "ubi0:rootfs" or unknown-block(0,0)
[ 11.349212] Please append a correct "root=" boot option; here are the available partitions:
[ 11.358062] 1f00 128 mtdblock0 (driver?)
[ 11.363403] 1f01 128 mtdblock1 (driver?)
[ 11.368774] 1f02 128 mtdblock2 (driver?)
[ 11.374114] 1f03 128 mtdblock3 (driver?)
[ 11.379455] 1f04 1920 mtdblock4 (driver?)
[ 11.384796] 1f05 128 mtdblock5 (driver?)
[ 11.390136] 1f06 5120 mtdblock6 (driver?)
[ 11.395477] 1f07 123392 mtdblock7 (driver?)
[ 11.400817] Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(0,0)
[ 11.409545] Backtrace:
[ 11.412139] [<c0017854>] (dump_backtrace+0x0/0x110) from [<c0422ca0>] (dump_stack+0x18/0x1c)
[ 11.421051] r6:00008000 r5:c05056d0 r4:c06a9d48 r3:c0660d48
[ 11.427062] [<c0422c88>] (dump_stack+0x0/0x1c) from [<c0422eb8>] (panic+0x74/0x190)
[ 11.435180] [<c0422e44>] (panic+0x0/0x190) from [<c05a6cd0>] (mount_block_root+0x198/0x228)
[ 11.443969] r3:c0660d48 r2:00000000 r1:cf01df60 r0:c05056d0
[ 11.449981] r7:c05d4b34
[ 11.452667] [<c05a6b38>] (mount_block_root+0x0/0x228) from [<c05a6fe4>] (prepare_namespace+0xb0/0x1d0)
[ 11.462493] [<c05a6f34>] (prepare_namespace+0x0/0x1d0) from [<c05a6948>] (kernel_init+0x124/0x128)
[ 11.471954] r6:c0041cdc r5:c063d164 r4:c063d164
[ 11.476898] [<c05a6824>] (kernel_init+0x0/0x128) from [<c0041cdc>] (do_exit+0x0/0x678)
[ 11.485229] r5:c05a6824 r4:00000000
[ 11.662322] ti81xx_interrupt 1146: VBUS error workaround (delay coming)
[ 13.654602] ti81xx_interrupt 1146: VBUS error workaround (delay coming)