大家好:
请问AM625这款产品是否支持IEC60730安全认证,是否能提供相关文档来协助进行这部分设计?
此外都支持哪些安全认证标准?
期待您的回复,谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
We do not provide certification for TI provided hardware or software to the IEC 60730 Class B and UL 1998 Class 1 and this is typically done at the system level. Requirements in these specs are derived from the IEC 61508 and the device will be certified for IEC 61508 SIL-2/ISO-26262 ASIL-B (systematic capability of ASIL-D/SIL-3).
The various features we support for the M4 MCU and IPs within the MCU channel satisfies the recommendations provided by the IEC 60730 and UL 1998 safety standards. Also select components of software provided by TI is developed with standards to meet functional safety requirements.