This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VL-Q1: CCS 12.4 通过USB无法与MCU建立连接

Part Number: TDA4VL-Q1

环境: VMware 16 + TDA4 VL SDK 8.6.1.3 + CCS12.4.0 + USB560 v2 System Trace调试器

问题: 在通过CCS的scripting console ,运行launch.js脚本时,提示错误。

经过分析,是脚本的dsMCU1_0 = debugServer.openSession( ".*MCU_Cortex_R5_0" );连接失败。

此外,在window10平台,也安装了CCS 12.4版本,运行会报如下错误:

驱动安装正确:

能帮忙分析一下哪里的问题吗?