我们使用单板使用2片 TDC7201ZAXR作为我们的时间测距模块,年用量5000PCS左右,数量大,出现了TDC的start引脚对地短路的情况。其中另一片的一个通道不使用,CSB2引脚我们连接上拉电阻接D3V3,也出现过该引脚对地短路的情况。出现这些都是在单板从焊接厂回来的单板测试阶段,还没有进入整机装机流程。因此可以推测是静电导致的损坏可能性比较大。
1. 请教一下,该芯片如何在引脚外围做防护?
2.另外一个不用的通道的每一个引脚,该如何处理?下图是我们的实际电路,是否有问题。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我们使用单板使用2片 TDC7201ZAXR作为我们的时间测距模块,年用量5000PCS左右,数量大,出现了TDC的start引脚对地短路的情况。其中另一片的一个通道不使用,CSB2引脚我们连接上拉电阻接D3V3,也出现过该引脚对地短路的情况。出现这些都是在单板从焊接厂回来的单板测试阶段,还没有进入整机装机流程。因此可以推测是静电导致的损坏可能性比较大。
1. 请教一下,该芯片如何在引脚外围做防护?
2.另外一个不用的通道的每一个引脚,该如何处理?下图是我们的实际电路,是否有问题。
您好,
1、start管脚和CSB管脚在电路板上是不是都引至了接线端子上?如果怀疑是静电导致的损坏,那么请考虑在接口处添加ESD管进行保护,所有的输入管脚最大耐压是VDD+0.3V.
2、您可以参考EVM 原理图设计电路图,我看到EVM电路图中每个管脚都有默认状态连接,TDC7201-ZAX-EVM User’s Guide (Rev. A):
https://www.ti.com.cn/cn/lit/ug/snau198a/snau198a.pdf