This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMP451-Q1: 器件AC时序测试参考值求助

Part Number: TMP451-Q1

Hi all,

我这边选用了TMP451-Q1作为车规级温度传感器的选型,在回片测试用例中遇到了一个问题:器件手册中未给出各个指标测量时对应的标准,比如对于上升时间测量,我们是从20%-80%作为上升沿测量标准还是30%-70%?

我需要这些标准用于I2C接口测试,可以帮我看一下是否有相关测试报告可以提供吗?谢谢!