我使用iwr6843isk-ods搭配mmwaveboost和DCA 1000EVM来采集雷达数据,看到手册里面有提到这款天线的接收天线1,4和2,3之间存在一个180°的相位差,想知道这是什么原因导致的,以及我该如何在处理端修正这个相位差。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我使用iwr6843isk-ods搭配mmwaveboost和DCA 1000EVM来采集雷达数据,看到手册里面有提到这款天线的接收天线1,4和2,3之间存在一个180°的相位差,想知道这是什么原因导致的,以及我该如何在处理端修正这个相位差。
这个相位差是由天线布线引起的。请看下面文档里的说明。
Line Feed: The RX line feeds on xWR6843AOP ES2 are same as on ES1 i.e. RX1 and RX2 are fed from opposite ends, which results in a 180° phase difference between RX1 and RX2. Similarly, RX3 and RX4 are out of phase by 180°.
https://www.ti.com/lit/an/swra656c/swra656c.pdf
如何补偿见文档说明。
RX Channel Phase Compensation: To compensate for the opposite line feeds as shown in Section 5.12, a 180° phase inversion is applied to the corresponding RX channels (including virtual channels) using the compRangeBiasAndRxChanPhase CLI command available in the mmw demo.