This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR2944EVM: i want to know Whether the2944 device supports advanced chirp configuration?

Part Number: AWR2944EVM

how to use these api such as  rlSetAdvChirpConfig(),rlSetAdvChirpLUTConfig?

  • Hello,

    RlSetAdvChirpConfig(): This API is used to configure advanced chirp parameters for radar. Chirp is a type of signal used for transmission in radar systems, and its frequency increases linearly with time. When calling this API, you need to provide a structural parameter that includes configuration information for chirp, such as starting frequency, bandwidth, slope, pulse width, etc.
    RlSetAdvChirpLUTConfig(): This API is used to configure the Chirp Lookup Table (LUT) for radar. This is an advanced feature used to define complex chirp sequences, allowing users to define a series of chirp parameters, and the radar will emit chirps in the order specified in this lookup table. When calling this API, it is also necessary to provide a structural parameter that includes the chirp configuration information for each entry in the lookup table.

    Regards,

    Gary

  • does 2944EVM ES1.0 supports advanced chirp configuration?, the SDK version used is mmwave_mcuplus_sdk_04_02_00_02,
    and is there some examples about the advanced chirp configuration of 2944 ,i only find examples of 2243

  • Hello,

    New questions, please repost. Thank you for your understanding. Thank you

    Regards,

    Gary