你好,
如标题,我们在使用OPT3101,使用的是SUPER HDR 模式,校准后有1%的产品出现0.2米内距离偏差大(0.1米实际测试为0.3~0.4米),分析为问题产品在近距离时使用的不是小电流而是大电流。
请帮忙分析下问题,谢谢!
我们的配置参数如下:
void OPT3101::device::initialize(void){
// List of registers to initialize OPT3101 device after power-up
this->reg.force_en_slave = 1; // //Since I2C Master bus is floating this register needs to be set to enable device to respond
this->reg.tg_ovl_window_start = 7000; // //Overload flab observation window
this->reg.en_temp_conv = 1; // //Enables the internal
this->reg.clip_mode_fc = 1; // //Enables Clip mode for Frequency correction
this->reg.clip_mode_temp = 0; // //Disables Clip mode for Temp coff phase correction
this->reg.clip_mode_offset = 0; // //Disables Clip mode for phase offset correction
this->reg.iq_read_data_sel = 3; // //Enables 16 bit frame counter
this->reg.iamb_max_sel = 12; // //Sets maximum ambient support
this->reg.en_temp_corr = 1; // //Enables Temperature Correction
this->reg.gpio1_obuf_en=1; // //Enabled output buffer on GPIO1 pin
this->reg.gpo1_mux_sel=2; // //select dig_gpo_0 on gpio1
this->reg.dig_gpo_sel0 = 9; // //Select Data Ready on dig_gpo_0
this->reg.num_sub_frames = 79; // //Sub frames count
this->reg.num_avg_sub_frames = 63; // //Average frames count
this->reg.xtalk_filt_time_const = 4; // //Crosstalk filter time constant
this->reg.tg_seq_int_start = 9850; // //Sequence Start
this->reg.tg_seq_int_end = 9858; // //Sequence End
this->reg.tg_seq_int_mask_start = 63; // //Same as AvgFrame Count
this->reg.tg_seq_int_mask_end = 63; // //Same as AvgFrame Count
this->reg.command0 = 0x108; // //Set Channel 1
this->reg.command1 = 0xB02; // //COMP1.
this->reg.command2 = 0x100; // //Set Channel 0
this->reg.command3 = 0xC00; // //COMP1_INV
this->reg.compare_reg1 = 26000; // //ThresholdH
this->reg.compare_reg2 = 4312; // //ThresholdH
this->reg.mux_sel_compin = 0; // //Selects Amplitude for Comparison
this->reg.en_tx1_on_tx0 = 1; // //Setting TX1 register and connect to TX0
this->reg.en_processor_values = 1; // //Enables processor values
this->reg.en_sequencer = 1; // //Enables the Sequencer
this->reg.hdr_thr_high = 25500; // //High Threshold
this->reg.hdr_thr_low = 4812; // //Low Threshold
this->reg.en_adaptive_hdr = 1; // //Enables adaptive HDR feature
this->reg.illum_dac_h_tx0 = 7; // //High Current settings [009.8mA:1.4mA X 07]
this->reg.illum_scale_h_tx0 = 3; // //Illum scale for H [009.8mA:1.4mA X 07]
this->reg.illum_dac_l_tx0 = 1; // //High Current settings [002.8mA:2.8mA X 01]
this->reg.illum_scale_l_tx0 = 2; // //Illum scale for H [002.8mA:2.8mA X 01]
this->reg.illum_dac_h_tx1 = 28; // //High Current settings [156.8mA:5.6mA X 28]
this->reg.illum_scale_h_tx1 = 0; // //Illum scale for H [156.8mA:5.6mA X 28]
this->reg.illum_dac_l_tx1 = 7; // //High Current settings [039.2mA:5.6mA X 07]
this->reg.illum_scale_l_tx1 = 0; // //Illum scale for H [039.2mA:5.6mA X 07]
this->reg.tg_en = 1; // //Enables Timing Generator
this->configurationFlags_xtalkFilterTau = 4; // //This is not a register but a settings flag for the SDK
this->configurationFlags_monoshotMode = false; // //This is not a register but a settings flag for the SDK
this->configurationFlags_xtalkSettlingOneTauInMilliSeconds = 320; // //This is not a register but a settings flag for the SDK
this->configurationFlags_xtalkSettlingOneTauInDataReadyCounts = 16; // //This is not a register but a settings flag for the SDK
this->configurationFlags_frameTimeInMilliSeconds = 20; // //This is not a register but a settings flag for the SDK
this->configurationFlags_avgFrameCountExponentOfTwo = 6; // //This is not a register but a settings flag for the SDK
}
OPT3101::device::device(void):
configurationFlags_isTXChannelActive{true,true,false},
configurationFlags_isRegisterSetActive{true,true} {}
OPT3101::calibrationC::calibrationC(void) : calibrationC(true) {
this->recordLength = 4; // //This configuration requires 4 crosstalk and other configuration record(s)
this->registerAddressListSize= 36; // //This configuration requires 36 registers [1152] bits to be stored for calibration
this->EEPROM_connected = false; // //This configuration helps configure EEPROM
this->extTempSensor_connected= true; // //This configuration helps configure Ext temp sensor
this->registerAddressList[0] = 0x2f; // //Address for register(s) iphase_xtalk_reg_hdr0_tx0,temp_coeff_main_hdr1_tx1
this->registerAddressList[1] = 0x30; // //Address for register(s) qphase_xtalk_reg_hdr0_tx0,temp_coeff_main_hdr1_tx1
this->registerAddressList[2] = 0x38; // //Address for register(s) temp_coeff_xtalk_iphase_hdr0_tx0
this->registerAddressList[3] = 0x39; // //Address for register(s) temp_coeff_xtalk_qphase_hdr0_tx0
this->registerAddressList[4] = 0x42; // //Address for register(s) phase_offset_hdr0_tx0
this->registerAddressList[5] = 0x47; // //Address for register(s) tmain_calib_hdr0_tx0,tillum_calib_hdr0_tx0
this->registerAddressList[6] = 0x45; // //Address for register(s) temp_coeff_main_hdr0_tx0
this->registerAddressList[7] = 0x46; // //Address for register(s) temp_coeff_illum_hdr0_tx0
this->registerAddressList[8] = 0x31; // //Address for register(s) iphase_xtalk_reg_hdr1_tx0
this->registerAddressList[9] = 0x32; // //Address for register(s) qphase_xtalk_reg_hdr1_tx0
this->registerAddressList[10] = 0x5e; // //Address for register(s) temp_coeff_xtalk_iphase_hdr1_tx0,temp_coeff_xtalk_iphase_hdr0_tx1
this->registerAddressList[11] = 0x60; // //Address for register(s) temp_coeff_xtalk_qphase_hdr1_tx0,temp_coeff_xtalk_qphase_hdr0_tx1,temp_coeff_xtalk_qphase_hdr1_tx1
this->registerAddressList[12] = 0x51; // //Address for register(s) phase_offset_hdr1_tx0,temp_coeff_illum_hdr1_tx0
this->registerAddressList[13] = 0x48; // //Address for register(s) tmain_calib_hdr1_tx0,tillum_calib_hdr1_tx0
this->registerAddressList[14] = 0x2d; // //Address for register(s) temp_coeff_main_hdr1_tx0,temp_coeff_main_hdr0_tx1
this->registerAddressList[15] = 0x52; // //Address for register(s) temp_coeff_illum_hdr1_tx0,phase_offset_hdr0_tx1
this->registerAddressList[16] = 0x33; // //Address for register(s) iphase_xtalk_reg_hdr0_tx1
this->registerAddressList[17] = 0x34; // //Address for register(s) qphase_xtalk_reg_hdr0_tx1
this->registerAddressList[18] = 0x49; // //Address for register(s) tmain_calib_hdr0_tx1,tillum_calib_hdr0_tx1
this->registerAddressList[19] = 0x53; // //Address for register(s) temp_coeff_illum_hdr0_tx1,phase_offset_hdr1_tx1
this->registerAddressList[20] = 0x54; // //Address for register(s) temp_coeff_illum_hdr0_tx1
this->registerAddressList[21] = 0x35; // //Address for register(s) iphase_xtalk_reg_hdr1_tx1
this->registerAddressList[22] = 0x36; // //Address for register(s) qphase_xtalk_reg_hdr1_tx1
this->registerAddressList[23] = 0x5f; // //Address for register(s) temp_coeff_xtalk_iphase_hdr1_tx1
this->registerAddressList[24] = 0x41; // //Address for register(s) tmain_calib_hdr1_tx1
this->registerAddressList[25] = 0x43; // //Address for register(s) tillum_calib_hdr1_tx1,en_phase_corr,en_temp_corr,scale_phase_temp_coeff
this->registerAddressList[26] = 0x55; // //Address for register(s) temp_coeff_illum_hdr1_tx1
this->registerAddressList[27] = 0x56; // //Address for register(s) temp_coeff_illum_hdr1_tx1
this->registerAddressList[28] = 0x2e; // //Address for register(s) illum_xtalk_reg_scale
this->registerAddressList[29] = 0x3a; // //Address for register(s) scale_temp_coeff_xtalk
this->registerAddressList[30] = 0x71; // //Address for register(s) shift_illum_phase
this->registerAddressList[31] = 0xb5; // //Address for register(s) scale_amb_phase_corr_coeff
this->registerAddressList[32] = 0x0c; // //Address for register(s) amb_phase_corr_pwl_coeff0
this->registerAddressList[33] = 0xb4; // //Address for register(s) amb_phase_corr_pwl_coeff1,amb_phase_corr_pwl_coeff2,amb_phase_corr_pwl_coeff3
this->registerAddressList[34] = 0xb8; // //Address for register(s) amb_phase_corr_pwl_x0,amb_phase_corr_pwl_x1
this->registerAddressList[35] = 0xb9; // //Address for register(s) amb_phase_corr_pwl_x2
}