This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMCS1101: 关于此芯片输入信号带宽的问题input signal bandwidth for this chip

Part Number: TMCS1101

手册上写的是信号带宽是80KHZ,应该是输入到输出之间的频率响应能达到的带宽,请问输入引脚IN+和IN-之间的信号有带宽限制吗,因为我们使用此芯片时在空载情况下会通过大概几十MHZ的信号,会对此信号造成影响吗

The manual states that the signal bandwidth is 80KHZ. Is there a bandwidth limit for the signal between input pins IN+and IN -?

  • 感谢您对TI产品的关注!
    关于你的咨询,TMCS1101 的Bandwidth通常指的是电流传感器能够准确响应的输入信号频率范围80KHz。
    如果输入信号的频率超过了TMCS1101的带宽80KHz,那么芯片可能无法准确地测量或传输该信号,导致输出信号失真或误差。
    对于几十MHz的信号,有可能出现下面的几种情况。
    但是,下面仅是理论情况,具体是否会出现,请以实际测量为准。

    误差增加:输出信号可能会失真,导致测量误差增加。
    噪声增加:高频噪声可能会对测量产生更大的影响。
    信号失真:信号的幅度、相位或形状可能会发生变化。

    如果你的几十MHz的信号没什么用的话,前端可以加filter过滤下。