This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMUX6219-Q1: TMUX6219-Q1 S1引脚电压比VDD电压高1.6V会有什么影响

Part Number: TMUX6219-Q1

TMUX6219DGKRQ1这个器件,如果器件的S1引脚的电压被拉高为12.6V,但是VDD供电电压为11V,这会对器件的功能、漏电、可靠性以及寿命方面有什么影响吗?

手册内部说IO会有一个钳位到VDD的二极管,这个二极管Vf电压是多少?

  • 您好,

    已经收到了您的案例,调查需要些时间,感谢您的耐心等待。

  • 源极/漏极引脚限制为VSS-0.5V至VDD+0.5V,最大安全电压为11.5V。施加12.6V(与信号S1一样)超过此限制1.1V。“引脚是二极管箝位到电源轨上的。过电压信号的电压和电流必须限制在最大额定值。”超过最大额定值可能会扭曲信号完整性,并可能导致电源VDD反向。
    长时间的过电压应力会降低片上ESD保护,影响器件可靠性。