请问TMUX154E这个开关能通过0-5V的正弦波吗? 频率是大约200MHz,会产生衰减吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
TMUX154E这个开关不能通过0-5V的信号,最大只能到VCC,而VCC供电范围是4.3Vmax
您可以看下TMUX1136 ,如下截图,它的供电电压可以到5.5V,可以通过0~5V的信号,它的-3dB带宽是220MHZ
或者具有断电保护功能的 5V、2:1 (SPDT)、2 通道模拟开关 TMUX1072 ,带宽为1200MHZ
具有下冲和过充电压保护的 5V、2:1 (SPDT)、2 通道模拟开关 TS5A623157 带宽 371 MHz
您输入的信号频率范围是多少?还是就一直是200MHz?
因为TMUX154E是CMOS输入,对输入信号的斜率或者说速度有要求,查看下面截图蓝色框内,这个文档Implications of Slow or Floating CMOS Inputs (SCBA004)有对输入要求的解释,简单来说就是TMUX154E是CMOS输入,如果输入信号比较慢(上升沿或下降沿比较缓),那么就可能使CMOS输入结构里的上管和下管同时导通,电源相当于直接加在上管和下管上,可能会烧掉芯片
但是datasheet中又没有说明对输入信号上升时间的要求,如果您输入的信号频率在一个比较高的范围内,我就去确认一下这个芯片对输入信号上升时间的要求