您好:
我有一气体流量计项目打算选取一款1-5V 转 4-20mA 的压流转换芯片,精度要求小于±0.5%F.S.能否帮忙推荐一款适合的芯片或者方案
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好:
我有一气体流量计项目打算选取一款1-5V 转 4-20mA 的压流转换芯片,精度要求小于±0.5%F.S.能否帮忙推荐一款适合的芯片或者方案
您好,可以选择XTR115这款4~20mA transmitter。
Io= 4mA~20mA,则Iin= 40µA ~ 200µA。因此Rin=25Kohm,Vin的范围为1V~5V。