Q1.請問使用PMP20497 的相同線路與相同規格PA4826NL 的變壓器,可以輸入DC12V到DC57V,輸出54V@2A嗎?
Q2.PA4826NL變壓器一次側線圈電壓可以承受57V輸入嗎?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
这个设计是针对12V(11~13V)输入的设计,但是实际输入电压增加并没有问题,在 设计时,变压器考虑的是最低输入电压(此时 电流最大),而不会是最高输入电压,变压器能承受。